浏览常见问题解答

Galaxy 3500, Smart-UPS VT and AIS3000 Power Factor Information

发布日期: 24 January 2018

Issue:
Galaxy 3500, Smart-UPS VT and AIS3000 Power Factor Information

 
Product line:
Galaxy 3500, Smart-UPS VT and AIS3000
 
 
Environment:
All models/ all serial numbers
 
 
Cause:
Galaxy 3500, Smart-UPS VT and AIS3000 Power Factor Information
 

Resolution:
"The SUVT and the AIS3000 have an Input Power Factor Correction Module which corrects the Power Factor on the input of the unit. The Input Power Factor is 1. There is no phase shift between voltage and current on the input, which minimizes the installation costs by enabling the use of smaller size cabling.

The Output Power Factor is 0.8 - what means that, for example, a 10KVA unit can provide a maximum total load of 8KW. This means there is a difference of 20% between real and apparent power.

Refer to the following application note for a better understanding of power factor as related to APC products

https://www.apc.com/salestools/SADE-5TNQYL/SADE-5TNQYL_R1_EN.pdf

 


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。