浏览常见问题解答

InfrastruXure (ISX) Manager Reports "Bank" Current as "Phase" Current for Certain Rack PDUs

发布日期: 18 December 2013

Issue

Bank current is showing as phase current within the InfrastruXure (ISX) Manager data log


Product Line

  • InfrastruXure (ISX) Manager - AP92200

  • Rack Power Distribution Unit models:
    • AP7802
    • AP7811
    • AP7822
    • AP7832
    • AP7832J
    • AP7841
    • AP7853
    • AP7902
    • AP7902J
    • AP7911
    • AP7922
    • AP7932
    • AP7932J
    • AP7941
    • AP7853

Environment

  • All serial numbers
  • All ISX Manager versions
  • All Rack PDU firmware versions

Cause


For certain single phase Rack Mount Power Distribution Units with multiple banks of outlets, the ISX Manager will list their current by "phase" instead of by "bank" in the Data Log.

This means that Bank #1 will be listed as "L1" and Bank #2 will be listed as"L2," even though all current is being supplied on the same electrical phase. L3 in the log will be the total current draw from both banks.

All alarms related to this labeling issue will also report the term as phase and not bank. All values reported in the logs are correct apart for the labels (Phase vs Bank).


Resolution



Make note of the labeling discrepancy



对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。