浏览常见问题解答

Device Identification Fields in InfraStruXure (ISX) Manager Report as "Unknown"

发布日期: 09 October 2013


Issue

Device Identification Fields in InfraStruXure (ISX) Manager Report as "Unknown"


Product Line
  • InfrastruXure (ISX) Manager - AP92200


Environment
  • Various versions of ISX Manager as noted

Cause

For every device the InfraStruXure Manager monitors there is a "Device Identification" option which lists three properties for identifying a device. These three properties are "System Name," "Contact," and "Location." To view or configure these properties right-click on the desired device and select "Device Identification."


Resolution

There are a couple of reasons why these fields may appear as "Unknown."
  • The ISX Manager is doing an SNMP get for the corresponding identification settings that have been configured on the Network Management Card (NMC) that the ISX Manager is monitoring. If these have not been set on the NMC then they will appear as "Unknown" in the ISX Manager as "Unknown" is the default value on the NMC for these fields. These fields can then be configured either on the NMC or the ISX Manager to the desired values.
  • On older revisions of the ISX manager (4.3 and below), Symmetra and Silcon UPS units communicate differently than any other APC products. This communication doesn't support the transfer of the Device Identification fields from the card to the manager or vice versa. The device identification fields for these devices will either have to be configured individually in both the NMC and ISX Manager or ISX Manager will need to be updated to at least version 4.4.


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。