浏览常见问题解答

Smart-UPS VT-G3500; what is Generator Charge (GEN CHRG) mode feature, how does it work?

发布日期: 16 October 2018

Issue:
What is Generator Charge (GEN CHRG) mode feature, how does it work?

 
Product line:
Smart-UPS VT – Galaxy 3500

 
Environment:
All Product models, All serial numbers

 
Cause:
Generator Charge is for de-rating the power the UPS uses for charging the battery when supplied from a generator.

 
Resolution:
The GEN CHRG (Generator Charge) mode can be activated via the display: Main Menu>System>Gen Chrg. The generator must supply a signal to the UPS to reduce charge.
 
UPS TB J106, Pins 7 & 8 are for external charge control. When 7 & 8 are closed, the UPS charges batteries with a pre-defined percentage (0-100%) of the maximum charging power. To be used in generator applications, or if special codes requires control of charging. See page 36 attached file, install guide.

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。