浏览常见问题解答

Video: How to mount a Rack Mount Symmetra or Rack Mount Smart-UPS to a 2 Post Rack?

发布日期: 14 September 2020

Issue:
Mounting a Rack Mount Symmetra or Rack Mount Smart-UPS to a 2 Post Rack    

Product Line:
Smart-UPS, Smart-UPS Online, Symmetra

Environment:
All rack mount models, All Serial Numbers

Cause:
Some users may be using a 2 post rack instead of a standard 4 post IT Rack.

Resolution:
We offer 2 post Rack Mount Kits for Smart-UPS, Smart-UPS Online, and Symmetra units.

AP9625:

  • All Rackmount Smart-UPS 2U or larger in height, as well as associated external battery packs

  • The following Symmetra models: SYH2K6RMT-, SYH4K6RMT-, SY6K6RMT-, SY8K12RMT-, SY12K12RMT-, SYH2K6RMi, SYH4K6RMi, SY6K6RMi, SY8K12RMi, SY12K12RMi

  • All 2U Step down Transformers (Including models bundled with SURT and SRT Smart-UPS Online Products)

  • All Smart-UPS Online SURT models 10Kva or less and associated external battery packs (NOTE: If your UPS is not a Rackmount model you will also need the SURTRK or SURTRK2 rail kit in addition to the AP9625)


SRTRK3:

  • All Smart-UPS Online SRT models and associated external battery packs

 

SYOPT12:

  • All Smart-UPS Online SURT models larger than 10Kva (These units are 2 modules and require Qty2 SYOPT12)
  • All Symmetra LX




 

The 2 Post rack kits all install the same way:

  • Install Rackmount ears on the front of the UPS
  • Attach 2 rails to the front of the rack using included screws
  • Attach 2 rails to the back of the rack using included screws
  • Slide UPS into rail kit and secure ears to rails using included screws
NOTE: You must use a separate rack kit for each piece of equipment.

The following video demonstrates how to install a two post rack kit:


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。