浏览常见问题解答

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

发布日期: 04 June 2019


Issue

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

Product Line
 

  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
 
  • UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH
     


Environment
 
  • All serial numbers
  • All firmware versions
  • SNMPv1 or v3 traps


Cause

SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type. 


Resolution

Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.

 


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。