浏览常见问题解答

Which UPS models are compatible with AP9622 Modbus/Building Management Integration Card? Where are the UPS bit registers AP9622?

发布日期: 04 June 2019



Issue

Which UPS models are compatible with AP9622?

Where are the UPS bit registers for my Building Management Integration Card (AP9622)?



Product Line
 
  • UPS Device Management
    • AP9622 - RS-232 Modbus/JBUS Building Management Integration SmartSlot Card

Environment
 
  • All serial numbers
  • AP9622 applications

Cause

This article provides general reference material and compatibility information.


Resolution


The AP9622 supports the following UPS series:
  • Smart-UPS (SU, SUA, SUM)
  • Smart-UPS RT (SURT, SURTA),
  • Matrix
  • Symmetra (single and three phase)
  • Smart-UPS VT/Galaxy 3500
  • Silcon
  • AIS


Note: The Galaxy 3500 UPS is supported by the AP9622, however some specific Symmetra 3-phase registers may report back but others will not work properly unless in a 3:3 configuration.



Note: Smart-UPS VT, AIS3000, and SURT15K/SURT20K units use the Symmetra maps and AIS5000 uses the Silcon maps.



Bit map registers are available on the APC website under the Documentation tab: https://www.apc.com/shop/no/en/products/Modbus-Jbus-Interface-Card/P-AP9622
 

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。