浏览常见问题解答



Matrix-UPS emits a chirping sound after being on-battery or running a self-test
If a SmartCell battery pack fails a UPS On-Battery Self-test (either scheduled or through UPS start-up), the Matrix-UPS will emit chirps for an interval of one minute to warn of a Replace Battery condition.
How Does Matrix-UPS Report Output Voltage?
The factory default for Out V Report is Auto; in this mode the Matrix-UPS reports its output with respect to its input voltage selection (set manually inside the UPS by the user at start-up).
Video: Battery Installation of APC AV Power Conditioners with Battery Back-Up
How to install and connect the battery in a APC Power Conditioner with Battery Back-Up at first time start-up or following routine battery replacement.
Battery Discharge During Storage
Depending on the health of the batteries, they can discharge below start-up voltage (approximately 85vdc) within 72 hours if the UPS is not operating normally.
The use of non computer type loads with a UPS, specific to Back-UPS, Smart-UPS SC
Ensure that the Volt Amp rating of the UPS is sufficient to handle the start-up inrush current draw of the motor.
NetBotz 750 | Accessing the Web User Interface (Web UI)
NOTE: The Web UI takes about six minutes to become available after start-up.
APC UPS Network Management Card (NMC) Compatibility Chart
When the card is installed after the UPS, however, a new Start-up service (WSTRTUP-VS1-a50) needs to be purchased to upgrade the UPS and the card at the customer site.
What are your condenser clearances and placement requirements?
Condensers also may require additional wiring to power the recive heaters, this can be reviewed upon start-up
NetBotz 455 | Physical Description
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
NetBotz 450/550/570 | Physical Description
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).


结果 1 - 10 11

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。