浏览常见问题解答



How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
In order to setup the external battery packs, please key in as (Ah of battery) x (total number of batteries).
PowerChute Business Edition 8.0.1 Agent cannot be scheduled to shutdown using the PowerChute Business Edition 8.5 Server and Console.
Scheduled shutdown is not supported on PCBE Server and Console 8.0.X with PCBE Agent version 8.5.X Solution:
HTTP/HTTPS Web Access does not work in v6.X.X firmware but works on v5.X.X in certain NMC2 configurations/environments
Users upgrading from v5.X.X firmware Users using a fresh install of v6.X.X firmware
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
All serial numbers All installations of v6.X.X firmware with the aforementioned applications
Why is the Environment Tab missing from the web interface on my AP9631 NMC2 v5.X.X firmware?
The firmware application is incorrect for the product that the AP9631 is installed in.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Q: What is the battery voltage that is required for SRC 5 and 6 KUXI Models? A: Requires a 192 Vdc battery system.
PowerChute Business Edition 8.5 and later Linux Package Signing Key
Issue: Installing the RPM distribution of PowerChute Business Edition Agent gives warnings or errors.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。