浏览常见问题解答



What's the vertical mounting rail depth for the NetShelter SX cabinets?
A unique "captive" vertical rail design prevents the rail from dislodging during the adjustment process.
Are the NetShelter SX and VX cabinets Zone 4 compliant, high seismic, IBC or NEBS?
The NetShelter SX product family, when using the ar7701a-S bolt-down kit and proper anchoring, meets IBC High Seismic Area specifications and OSHPD certification.
What is the IP (Internal Protection) rating of the NetShelter SX, SV and CX cabinets?
Issue: Internal Protection (IP) rating of the NetShelter SX, SV and CX cabinets is required.
What are the differences between the NetShelter SX and the NetShelter SX Networking cabinets?
Issue: There's a question what the differences are between the NetShelter SX and the NetShelter SX Networking cabinets.
What are the perforation pattern percentages of the NetShelter SX, SV or VX cabinet?
see attached file. There is also information in the NetShelter SX Bid Specifications document on the APC website.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。