浏览常见问题解答



Video: My Back-UPS emits a clicking sound, yet functions properly
Input Sensitivity Adjustment for Back-UPS Pro M2 & Sinewave Series (br1000ms/bn1100m2/bn1350m2/br1350ms/bn1500m2/br1500ms)
Back-UPS CS: Runtime does not exceed 45 minutes
The 120v and 230v International Back-UPS CS models bk350ei and bk500ei, that were made before January 1st 2004, have a max runtime limiting cap of 45 minutes.
How is the rackmount U-space of a NetShelter cabinet or rack identified?
1. For any Rackmount device or enclosure - a U or unit of rack space is equivalent to 1.75 inches or 44.45 mm.
MGE; Why my NMC (Network Management Card) stops logging new measurement information and new events?
Save current measurements logs and then delete wait a few seconds and new/ current logs will generate.
Smart-UPS C Series FAQ
They output a pure sinewave, are fully compatible with PFC power supplies, and feature a new LCD Interface.
INFORMATION BULLETIN - Interface Expander 2 SmartSlot Card Smart Signalling Information and Explanation
These UPS types begin with the following model prefixes and will have a RJ-45 style serial port, as noted:
APC Environmental Sensors FAQ
Q. What are the two supplied RJ-45 plugs used for in the A-Link ports of the AP9319?
Changing the Language of the Symmetra PowerView RM Display
a . Attach the RJ- 45 connector to the port on the rear of the PowerView RM interface.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。