浏览常见问题解答



Does the Heartbleed OpenSSL vulnerability affect APC products?
To recover, upgrade all instances of Network Shutdown Module for Windows to v3.07.02 (available @ and select "Software Upgrade - MGE Accessories" in the Software Filter and click submit.) and
Video: Back-UPS Pro M2 & RS with SineWave; Adjustment of unit battery transfer sensitivity
APC Back-UPS Pro M2 & RS with SineWave; Adjusting the battery transfer settings.
If we install the APC-MGE proposed leakage sensors AP9325/ 9326 , can we send dedicated notification via dry contact of this sensor to our BMS which knows modbus?
If we install the APC-MGE proposed leakage sensors AP9325/ 9326 , can we send dedicated notification via dry contact of this sensor to our BMS which knows modbus?
What third party products are supported by the APC Netbotz SNMP Crawler?
"The APC Netbotz product range has SNMP crawler support for APC products, MGE products, as well as third party manufacturers.
Does the Shellshock Vulnerability affect APC products?
MGE Network Management Cards (660xx) MGE Network Shutdown Module
Is there a NetShelter Accessory Compatibility Chart that shows which NetShelter accessories, UPS, PDU, Symmetra, NetBotz, Air or KVM fit into a specific cabinet?
All current NetShelter cabinets are listed horizontally across the top of the document. The accessories & products that install into the cabinets are listed vertically.
Where can I view the current NetShelter cabinets, racks and accessories? I there a catalogue available?
Our current NetShelter product family of racks, cabinets and accessories can be viewed here:


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。