浏览常见问题解答



Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Both the UPSs share the load equally but if one fails (either through developing a fault or being taken out of service for maintenance), the other UPS will take over powering the load.
Which service bypass panel should be used for single phase Symmetra UPS systems?
Resolution This table provides a reference as to which service bypass panel must be used for a single phase Symmetra system.
Bypass operation of Symmetra Power Array 3:1 (3-Phase Input / 1-Phase Output)
This is only applicable for loads above 12 KVA. For loads below 12 KVA you can use a 60 Amp Circuit breaker.
Frequently Asked Pre-Sales Questions for Remote Monitoring Services (RMS)
Click here for the APC Remote Monitoring Service brochure
Stacking limitations for single phase Symmetra and Matrix products
Although instructions are provided for these stacking options, APC always recommends the use of its field service group to complete these procedures. Please Note:
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
The 80ah inside the table is the default setting for 5kva/6kva (1 EXB: 16pcs of 5ah battery)
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
to issue an email test. Allow 1-2 minutes and check your email inbox/SPAM folder for the test email.
Configuring the Windows SNMP Agent for use with PowerChute Business Edition versions 9.2.1 and below
1 . Go to Control Panel->Administration Tools-> Services ->SNMP service . The following screen will appear.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。