浏览常见问题解答



Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
Furthermore, temperature preference and other user preferences are now configurable on a per user basis in v6.X.X, rather than using a global setting by the administrator in v5.X.X.
Video: Silent Installation of a Windows PowerChute Business Edition Agent versions 7.x - 9.2.1
version 9.5 and 10.x are agent only installations. Installation instruction can be found at this link
Netbotz version 3.x OID data returned by SNMP GET or WALK arrives in a different order than in previous versions of Botzware.
So even though an OID's element existed and was active on the target device, its data may never be captured by an SNMP GET ...
INFORMATION BULLETIN: Network Management Card 2 upgrade from v5.1.X to v6.0.6 incorrectly maps SMTP server information
Upon upgrading a v5.1.X management card to v6.0.X, SMTP server information gets mapped to the incorrect setting causing email to fail after the upgrade.
What are the potential results of using a Smart-UPS with X-10 equipment?
Issue: What are the potential results of using a Smart-UPS with X-10 equipment?
Using a UPS with X-10 Equipment
A possible solution is to install an X -10 isolator which prevents a UPS from filtering out these signals.
HTTP/HTTPS Web Access does not work in v6.X.X firmware but works on v5.X.X in certain NMC2 configurations/environments
Users upgrading from v5.X.X firmware Users using a fresh install of v6.X.X firmware
Why is the Environment Tab missing from the web interface on my AP9631 NMC2 v5.X.X firmware?
As long as the AOS is loaded properly and you have an AP9631 or AP9631 embedded product with v5.1.7 sumx or sy APPs, the information will be visible and and indicate whether or not it detects a sensor connected.
How is the rackmount U-space of a NetShelter cabinet or rack identified?
Vertical Hole spacing must follow a pattern of 5/8""-5/8""-1/2"" or 15.9mm-15.9mm-12.7mm


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。