浏览常见问题解答



Why is my APC by Schneider Electric UPS derated to 80% of the circuit's total capacity?
When installing an APC UPS or any electrical device, it is important to keep in mind the ampacity of the circuit into which it is connected.
Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw
Issue: This document describes the required input over current protection (circuit breaker) required when installing a Symmetra PX
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) ap9630/AP9631 UPS Compatibility
Within the global Data Center and Facility 3 Phase UPS product catalog, exists different varities of Symmetra PX including 20, 40, 48, 80, 96, 100, and 160 kVA models.
How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame?
The need may arise for there to be space between the UPS mainframe and XR frames i.e. if they cannot be installed in the same rack or enclosure.
Matrix-UPS frequently asked questions regarding installation, operation, and standards
Matrix-UPS Accessories mx3000, mx3000xr, mx5000, mx5000xr, smartcell, smartcell xr, tone, alarm, screen, panel, matrix ups, install, wire.
How to troubleshoot the "Check Battery Pack Connection" Matrix-UPS Alert Message
2.) For each Smartcell-XR attached to the UPS, check the four internal batteries for proper voltage.
Single Phase Symmetra XR Frame Compatibility
Due to some design differences, not every single phase Symmetra XR frame is compatible with every UPS system in the single phase Symmetra product family.
What do I gain with a Unity Output Power Factor (kW=kVA)?
Some APC 3-phase UPS products as well as newer single phase products(SRT6K) have an output rating of kW=kVA or Unity Power Factor.
What are the Matrix-UPS operating temperature limitations?
Please note that while the Matrix-UPS Electronics and Isolation units may operate in ambient temperatures up to 40c, the SmartCell and SmartCell XR battery systems should not be exposed to ambient temperatures above 30c.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。