浏览常见问题解答



Why does a battery weaken when not in use?
1. Battery charger setting. Faulty charging shortens a battery's service life.
What are the battery replacement options for the Smartcell battery pack?
In order to continue to support the use of the Matrix battery pack, APC ... refurbished sales and service of the SMARTCELL battery packs.
Replace Battery LED Flashing on an "SUA" or "SUM" Smart-UPS
In this You should immediately disconnect the battery connector and take the UPS out of service .
Battery Damage When Battery Is Left Discharged
VRLA batteries should recover fully in terms of capacity and service life if recharged within 72 hours following a discharge.
Used Battery Disposal Options
Please note that return shipping service is not provided for the RBC13, RBC14, or Symmetra replacement battery products.
Video: How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
Issue: The UPS indicates battery replacement is required or is providing insufficient runtime compared to when the UPS was first put into service .
Replacing the Battery in a 1st Generation Back-UPS Pro
Except for the battery, the unit contains no user serviceable parts. Repairs are performed only by factory trained service personnel.
Battery Discharge During Storage
... which are required to discharge the large capacitors inside the unit in order to protect service personnel.
How can I adjust the number of battery packs on a Smart-UPS XL?
the UPS service must be stopped. 2. From the Desktop, go to: Start |Programs | Accessories | HyperTerminal.
Why does my SMC Series Smart-UPS switch to battery when it encounters high voltage?
... attached load to higher voltages, however it will never expose your load to anything outside of CBEMA standards for acceptable input voltage.


结果 1 - 10 50

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。