浏览常见问题解答

英飞中央管理器使用的网络端口

发布日期: 27 五月 2013

英飞中央管理器通信时使用那些端口?

以下是在英飞中央管理器中应用的程序和相应得端口

注意:加星号的端口是可以改变的

进入端口:

*Port 80 (TCP/UDP) - HTTP Communication from NetBotz Appliances / ISX Central Console
*Port 443 (TCP) - HTTPS Communication from NetBotz Appliances / ISX Central Console
*Port 161(UDP), 162 (TCP/UDP)- SNMP Communication from SNMP Agent
*Port 502 (TCP/UDP)- Modbus TCP Communication from Modbus Device/Gateway


输出端口:

*Port 80 (TCP/UDP)- HTTP Communication to NetBotz Appliances / ISX Central Console / HTTP Post to Web Server
*Port 443 (TCP) - HTTPS Communication to NetBotz Appliances / ISX Central Console
*Port 161 (UDP), 162(TCP/UDP) - SNMP Communication to SNMP Agent
*Port 25 (TCP)- SMTP Communication to Email Server
Port 21 (TCP)- FTP Communication to FTP Server
Port 123 (UDP)- NTP Communication to NTP Server
Port 139 (TCP/UDP)- SMB Communication to NAS / SAN
Port 53 (TCP/UDP)- DNS Communication to DNS Server
Port 111 (TCP)- NFS Mount
Port 2049 (UDP)- NFS Communication to NAS / SAN
Port 6000 (TCP)- APC Proprietary Communications protocol for use with AP76xx outlet strips and gen1 PDU on private lan.
Port 445 (TCP)- CIFS Communication to NAS / SAN
Port 502 (TCP/UDP)- Modbus TCP output to Building Management System
 


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。