浏览常见问题解答

Netbotz V3 串口配置IP地址

发布日期: 05 十月 2012

"

使用NetbotzV3之前,必须设置一些基本参数。本文介绍了如何通过串口通讯方式配置IP,步骤如下:

1
.使用随机带的USB通讯线连接运行终端仿真程序的计算机和Netbotz
2
.启动终端仿真程序如HyperTerminal,设置串口参数为:38400bps, No Parity , 8 data bits , 1 stop bit , and No Flow Control (注意关闭其他使用串口的程序,如果有需要请安装usb转串口驱动,下载链接:http://www.ftdichip.com/Drivers/VCP.htm)
注:修改串口参数后,要断开并重新连接该会话(connection)之后,设置方生效。
3.
确认上述两步无误后,按回车键。
4.
输入 User Name root ,Password apc均为缺省设置。

显示界面如下:(请根据您的需求修改相关参数)

NetBotz BotzWare V3.2.1

Warning: system login through this interface without direction

from NetBotz Support will void your warranty.

netbotz355 login: root

Password:

Linux netbotz355 2.6.12 #307 Wed Oct 21 14:06:44 EDT 2009 ppc unknown

Welcome to NetBotz BotzWare V3.2.1

--------------------------------------------------------------------------

PRODUCT INFORMATION:

Model is NetBotz Wall Monitor

Version is V3_2_1_20091021_1401

CURRENT ETHERNET CONFIGURATION:

MTU is supported

Speed is autonegotiate

Hostname is netbotz355

DHCP is disabled

IP address on LAN is 0.0.0.0

LAN interface's subnet mask is 0.0.0.0

IP address of default gateway to other networks is 0.0.0.0

MTU is 1500

This board's MAC Address is 00:C0:B7:C3:5B:BC

CURRENT DNS CONFIGURATION:

Domain is

Primary DNS is

Secondary DNS is

Tertiary DNS is

--------------------------------------------------------------------------

To change any of this, press enter within 5 seconds

(M)odify any of this or (C)ontinue? [M] m 选择修改配置

For each of the following questions, you can press <Enter> to select the

value shown in braces, or you can enter a new value.

Enable ethernet interface? [Y] 启用网络配置

Speed? 0=auto, 1=100FD, 2=100HD, 3=10FD, 4=10HD [0]

Hostname? [netbotz355]

Use DHCP? [N]

Host IP address? [] *.*.*.* 配置IP

Subnet mask for LAN? []*.*.*.* 配置掩码

Gateway IP address? []*.*.*.* 配置网关

MTU? [1500]

Domain? (type 'e' for empty/dhcp) []

Primary DNS? (type 'e' for empty/dhcp) []

Secondary DNS? (type 'e' for empty/dhcp) []

Tertiary DNS? (type 'e' for empty/dhcp) []

Configuring DNS settings...done

Configuring ethernet settings..../etc/network/config-eth0 due to UPDATE

eth0: STOP

eth0: OPEN

BD rings initialised, RBASE=618220, TBASE=618420

Configuring eth0 with static ip 10.219.11.234

Done

配置好IP等后退出,使用网页或advance view软件登陆即可

"

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。