浏览常见问题解答

如何用计算机串口超级终端配置AP9617/AP9618/AP9619

发布日期: 05 十月 2012

"

使用AP9617,AP9618,AP9619之前,必须设置一些基本参数。本文介绍了如何通过串口通讯方式配置AP9617,AP9618,AP9619. 配置步骤如下:

1.使用940-0024C通讯线(网络管理卡附带)连接运行终端仿真程序的计算机和UPS。
2.如该计算机的串口(连接940-0024C通讯线)正被APC软件PowerChute Plus或其他程序使用,请关闭相关程序。 启动终端仿真程序如HyperTerminal,设置串口参数为:2400bps, No Parity , 8 data bits , 1 stop bit , and No Flow Control
注:修改串口参数后,要断开并重新连接该会话(connection)之后,设置方生效。
3.     确认上述两步无误后,按回车键。
4.     输入 User Name及 Password ,其缺省设置均为 apc。
5.     正确登录后,网络管理卡的管理界面将自动弹出。

显示界面如下:(请根据您的需求修改相关参数)
User Name : apc
Password  : ***


American Power Conversion               Network Management Card AOS      v2.1.1
(c) Copyright 2002 All Rights Reserved  Smart-UPS & Matrix-UPS APP       v2.1.0
-------------------------------------------------------------------------------
Name      : Unknown                                   Date : 12/11/2003
Contact   : Unknown                                   Time : 11:47:50
Location  : Unknown                                   User : Administrator
Up Time   : 0 Days 0 Hours 20 Minutes                 Stat : P+ N? A+

Environment : Threshold Violation Present, Contact Alarms Disabled, Relay
    Disabled
Smart-UPS 1000 named  : On Line

------- Control Console -------------------------------------------------------

     1- Device Manager
     2- Network
     3- System
     4- Logout

     <ESC>- Main Menu, <ENTER>- Refresh, <CTRL-L>- Event Log
> 2

------- Network ---------------------------------------------------------------

     1- TCP/IP
     2- DNS
     3- Ping Utility
     4- FTP Server
     5- Telnet/SSH
     6- Web/SSL/TLS
     7- WAP
     8- SNMP
     9- Email
    10- Syslog

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
> 1

------- TCP/IP ----------------------------------------------------------------

        Network not started. Currently making a BOOTP request...
        -----------------------------------------------------------------------
        MAC Address : 00 C0 B7 67 37 4C

     1- Boot Mode  : DHCP & BOOTP
     2- Advanced...

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
> 1

------- Boot Mode -------------------------------------------------------------

     1- DHCP & BOOTP
     2- DHCP only
     3- BOOTP only
     4- Manual

     <ESC>- Back, <ENTER>- Refresh
> 4

------- TCP/IP ----------------------------------------------------------------

        Network not started. Currently making a BOOTP request...
        -----------------------------------------------------------------------
        MAC Address : 00 C0 B7 67 37 4C

        * Changes will take effect on Logout.

     1- System IP      : 159.215.125.248
     2- Subnet Mask    : 255.255.255.0
     3- Default Gateway: 159.215.125.1
     4- Boot Mode      : Manual
     5- Advanced...

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
> 1
System IP : 159.215.125.248

------- TCP/IP ----------------------------------------------------------------

        Network not started. Currently making a BOOTP request...
        -----------------------------------------------------------------------
        MAC Address : 00 C0 B7 67 37 4C

        * Changes will take effect on Logout.

     1- System IP      : 159.215.125.248
     2- Subnet Mask    : 255.255.255.0
     3- Default Gateway: 159.215.125.1
     4- Boot Mode      : Manual
     5- Advanced...

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
> 5

------- Advanced... -----------------------------------------------------------

        Link is down.

     1- Host Name     : APC
     2- Domain Name   : somedomain.com
     3- Port Speed    : Auto-negotiation
     4- Accept Changes:

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
> 4

------- Advanced... -----------------------------------------------------------

        Link is down.

     1- Host Name     : APC
     2- Domain Name   : somedomain.com
     3- Port Speed    : Auto-negotiation
     4- Accept Changes: Success

     <ESC>- Back, <ENTER>- Refresh, <CTRL-L>- Event Log
>

需要注意的是TCP/IP的三个参数包括System IP,Default Gateway,Subnet Mask都必须设置,尤其网关Default Gateway不能为0.0.0.0,否则会导致网络不通。退出超级终端,则网络设置成功。
首先用ping 命令检查网络配置是否成功,如果不能Ping通,请将卡Reset,卡上有一个白色的Reset按钮,按一下,则卡重启,该重启只是卡重新加电而已,不会改变卡内的已有的任何设置。

"

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。