Consulter la FAQ

In the NetShelter WX 6U Vertical cabinet, must the included 2U UPS Mounting Bracket be used?

Date de publication : 16 October 2019

Issue:
It's unclear if the included 2U UPS Mounting Bracket must be used. 

Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The AR106V/VI ships with a 2U UPS Mounting Bracket. 

Resolution:

If the UPS is being installed into the cabinet prior to shipping, the 2U Mounting Bracket is required. 
If the cabinet is not shipping with the UPS installed, then the UPS may be installed with its own mounting brackets. 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.