Consulter la FAQ

NetBotz 455 | Physical Description

Date de publication : 28 July 2020

Issue:
   Physical Description of the NetBotz 455 and 455A

Product Line:
   NetBotz v3
      - Wall Monitor 455A (NBRK0455A)

Environment:
   NetBotz 455/455A (All firmware versions)

Resolution:

Physical Description - Front



 
Item Description
1 Vented internal sensors Vented opening for airflow, temperature, and humidity sensors.
2 Network link LED Shows the status of the network connection. Blinks to indicate network traffic (green = connected at 10 Mbps; yellow = connected at 100 Mbps).
3 Power LED Indicates whether the unit is receiving power (green = receiving power; dark = not receiving power)
4 Camera LED Blinks steadily when the integrated camera is active.
5 Alert LED Indicates the alert status of the system.  When more than one alert exists, the most severe will be indicated.
- Flashing once every eight seconds = Informational
- Flashing one very four seconds = Warning
- Flashing once every two seconds = Error
- Flashing once every second = Critical
- Flashing twice per second = Failure
6 Temperature display - Displays the current temperature from 0 to 99 in Centigrade or Fahrenheit. The Temperature reading comes from the internal temperature sensor. If the temperature exceeds 99, the display will flash 99.
- When the unit first receives power, displays the unique identifier number for one minute.
- If an alert exists, flashes at the same rate as the Alert LED.
- During firmware upgrade, displays 88.
7 Lens housing Must be removed to change the focus of the integrated camera.

Physical Description - Back
Item Description
1 Microphone jack Supports audio sensing, audio recording, and two-way audio. Maximum length of microphone cable: 3 m (9.8 ft).
2 Speaker jack Supports two-way audio.
Maximum length of speaker cable: 3 m (9.8 ft).
3 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays. Provides communications and power to the connected devices over standard CAT-5 cabling with straight-through wiring.
4 10/100 Base-T network port Provides for a 10/100 Base-T network connection and power through Power-over-Ethernet (PoE). (The appliance operates at 100 Base-T only.) Status and link LEDs indicate network traffic:
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
- Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps).
5 Sensor ports (4) Used for connecting APC by Schneider Electric sensors, third-party dry-contact sensors, and standard third-party 0-5 V sensors. Third-party dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304). Standard third-party 0-5 V sensors require the NetBotz 0-5 V Sensor Cable (NBES0305).
6 USB-A port Used to connect a USB device to the appliance.

The complete NetBotz 455 Installation and Quick Configuration Manual can be found here.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.