Consulter la FAQ

Using UPS Network Management Card 2 v6.2.0 sumx application to upgrade SMT UPS firmware via Internet Explorer may fail

Date de publication : 17 December 2014


Issue

While uploading a UPS firmware update to a SMT model UPS using UPS Network Management Card 2 sumx firmware application v6.2.0, Internet Explorer may prematurely drop the connection, causing the UPS firmware upgrade to fail.


Product Line
  • Smart-UPS tower models with SKUs beginning with "SMT" prefix
  • Smart-UPS 2U Rackmount models with SKUs beginning with "SMT" prefix
  • UPS Network Management Card 2 - AP9630/30CH, AP9631/31CH

Environment
  • UPS Network Management Card 2 firmware APP v6.2.0
  • UPS models listed above
  • Users upgrading UPS firmware through Internet Explorer web browser as outlined in knowledge base article ID FA170679

Cause

Firmware updates on the aforementioned UPS models are slow, and Internet Explorer has a timeout based on rate of transfer during uploading. This timeout varies between versions, within the same version, even for operations defined to have no timeout. No other browser Schneider Electric has tested including Firefox, Chrome, Safari, and Opera behaves this way. 


Resolution

It is recommended not to use Internet Explorer for UPS firmware upgrades via the Network Management Card. Use the FTP method (outlined in knowledge base article ID FA170679) or any other web browser. Schneider Electric is evaluating possible remedies to support Internet Explorer in the future for the UPS firmware upgrade via AP9630/31.

 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.