Consulter la FAQ



What type of battery could I use with the Galaxy VS UPS?
Galaxy VS , 3 Phase UPS , Uninterrupted Power Supply,10 kVA ,15 kVA ,20 kVA , 20 kVA , 30 kVA ,40kva, ... use with the Galaxy VS UPS ?, battery ...
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS , 3 Phase UPS , Uninterrupted Power Supply,10 kVA ,15 kVA ,20 kVA , 20 kVA , 30 kVA ,40kva, ...
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from normal operation ... Galaxy 5000, Galaxy 5500 ... request come in for assistance with Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... This procedure is for a single UPS with an external ... Step 1 : Touch any ... to wake it up . ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to ... ... protected by the UPS . Step 8 : Unlock CB2 ... The UPS is now fully ... ... : Open the UPS door. ... Turn off Q 1 Switch
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000, Galaxy 5500 For various reasons, the Galaxy 5000 may be ... ... This is not for commissioning a new UPS . ... of a new UPS must be performed ... ... to restore the Galaxy 5000 UPS from total power ... ... This procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC start- up . ... “Start the UPS Step 5 : Turn the ... Step 8 : Set the ... The Inverter Assumes the load, and the UPS is normal operation with the load protected.
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.
Does the NTP need to be configured on all NMCs for all parallel Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 ... request come in for assistance with Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... This procedure is for a single UPS without an external ... Step 1 : Touch any ... to wake it up . ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to ... ... protected by the UPS . The UPS is now fully ... Step 5 : Set the ... ... Turn the Q 1 Switch to Off There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
Wiring information for egx100 to any ... ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Wiring information for egx100 to any ... ... card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... ... card is RS232 for configuration. One is down ( ... all others are up . ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Smart-UPS VT and Galaxy 3500 Power Off, Bypass and Power on Procedures
Smart- UPS VT and Galaxy 3500 Power Off ... Smart- Ups VT, Galaxy 3500 Smart- Ups VT and Galaxy 3500 Power off ... UPS BYPASS PROCEDURE WITHOUT ... ... , select “ UPS into Bypass” ... ... on front of UPS to the vertical ... UPS is now in ... ... contact with the UPS . ... input feed to UPS UPS Bypass Procedure IF ... ... , select “ UPS into Bypass” ... ... maintenance bypass with UPS in static bypass ... Turn Q 1 to OFF position ... contact with the UPS . UPS POWER UP SEQUENCE WITHOUT BYPASS ... ... input power to UPS
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
or UPS Network Management Card v6. X . X Firmware for Smart- UPS & Galaxy 3500 with ap9630/31/35


Résultats 1 - 10 de 68

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.