Consulter la FAQ



Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
Serial port setting : for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
The 66061 JBUS/Modbus card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is 2 ...
Galaxy VX; How to configure the Network Communications options
Resolution: The network can be configured for the display and for the cards in Smart Slot 1 and
Galaxy VX; How to set up, stop or change the “Automatic Battery Test” option of the UPS
Galaxy VX - all ... Configuration > Battery > Test Set your preferred settings for the automatic battery test: ... Every 8 Weeks ... When all settings have been completed, tap ... to confirm your settings .
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX ? ... Galaxy VX ... How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX ? ... http://www.apcmedia.com/salestools/MBPN-A35JB8/MBPN-A35JB8_R 1 _EN.pdf?sdirect=true ... software) to have the UPS go to static bypass on EPO (default setting is no).
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 5 : Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch. ... Step 8 : Unlock CB2, remove the key, and place it in the key interlock. ... Turn off Q 1 Switch
Material Safety Data Sheet for LI-ION battery Module
LIB Battery, Galaxy VM- VX -VS, SYPX 500 , SYMW
Where can I find manual for Samsung Li-Ion Battery Solution
LIB Battery, Galaxy VM- VX -VS, SYPX 500 , SYMW
Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
... PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250- 500 kva , SUVT, ... , ais3000, Galaxy VM
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Configuring NTP on both Galaxy VS internal NMC and the optional AP9644 NMC can cause issues like excessive time stamp events in the log files ...


Résultats 1 - 10 de 55

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.