Consulter la FAQ



How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
... Configuration of SRC battery packs via the ... Batteries need to be ... Resolution : ... the number of battery strings through the ... 5 . Enter the ... number of attached battery packs. ... setup the external battery packs, please ... (Ah of battery ) x (total number of batteries ). ... 16pcs of 5ah battery in series ( ... ... of 100 AH batteries in series(for 5 KVA), ... is 100 AH x 16 pcs= ... ... 16pcs of 5ah battery in series ( ... ... 16pcs of 5ah battery ) ... 20pcs of 7ah battery ) ... 20pcs of 9ah battery ).
How can I adjust the number of battery packs on a Smart-UPS XL?
... how many external batteries are connected so ... ... can use external batteries . ... and have Smart Batteries . battery packs. Resolution : battery packs. batteries effects the runtime ... ... is running on battery power. ... number of external batteries . external battery packs ... the number of battery packs via a ... the UPS service must be stopped ... ... ..must install a ... 2400 baud, 8 data bits, ... 5 . Click on ... ... " Adds a battery pack ... number of external battery packs ... " Subtracts a battery pack ... number of external battery packs ... the number of battery packs via a ...
Troubleshooting steps to perform when "Please check that the USB cable between your battery backup and PC is properly connected" message or "Unknown Device" appears after a reboot of your computer.
... cable between your battery backup and PC ... ... BACK-UPS XS , BACK- ... ... the following APC Battery Back-UPS ... ... drivers can be installed from your corresponding ... Resolution : 5 . Cycle power ... 8 . Ensure that ... ... see listings as Batteries and Human Interface ... ... drivers are already installed . ... steps 1- 8 . 11. Reboot your PC. After reboot, did your PC recognize the UPS or are you still receiving the initial message of ""Please check that the USB cable between your battery backup and PC is properly connected""?
Video: What are the different sensitivity settings of a Smart-UPS?
Resolution : ... to on- battery operation to protect ... ... to on- battery operation. Battery longevity and service life of the ... ... will transfer at X percent THD. ... ... to on- battery operation. ... online to on battery transfer when the ... ... will transfer to battery power and watch ... ... will transfer to battery power and watch ... ... generally 6- 8 milliseconds. ... will transfer to battery power and watch ... They are generally 8 -10 milliseconds. ... In any sensitivity mode, a Smart-UPS will transfer to battery when the Frequency(Hz) is out of tolerance(+/- 5 %).
Why does Symmetra LX see only half of my installed battery modules?
The bottom intelligence module monitors battery bays 1, 3, 5 , 7, ... , 6, 8 , 10, &12.
How do I upgrade the firmware of an XU1K3LLXXRCC using a USB Thumb Drive?
During the upgrade process the UPS will not be able to provide battery backup in the event of a Power Outage Resolution : ... Step 5 Scroll down and select “ Install UPS Firmware” ... Display automatically pop ups with “Receiving Firmware Image X % Completed” Step 8 ... Display automatically pop ups with “ Installing Firmware X % Do Not Power Off”
What does the Force Negotiation setting achieve in the Network Management Card?
Resolution ... be the low battery signal time/low battery duration value by ... battery signal/low battery duration is a ... ... the NMC Low Battery Duration value, ... , if the battery duration time is ... ... the NMC Low Battery Duration field value ... ... v3. X , the Maximum ... ... values (low battery setting vs. ... ... line shutdown of 8 minutes on the ... have a low battery of 10 minutes ... ... with the On Battery event used as ... ... UPS is on battery . ... page for On Battery executes concurrently. Low battery duration: 5 . A 2 ...
PowerChute Network Shutdown continually shuts down the ESXi host following On Battery Shutdown and UPS turn off when A/C power has been restored in Advanced UPS Configuration.
VMware ESXi versions 4. x , and 5 . x ... PowerChute is installed on a physical Windows machine and configured for Advanced UPS Configuration. ... When there are ESXi hosts registered with the Main Outlet Group and a UPS turn off initiated event occurs PowerChute does not resolve the UPS Critical event after the UPS is turned back on. ... Resolution : Upgrade to PCNS version 4. x
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... .Net 2.0 is not pre- installed as part of the OS ... You will need to install the .Net 3.5 ... 5 . You should see .NET Framework 3.5 (includes .NET ... Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary). ... 2.0 you can now install PowerChute Personal Edition 3.0.2
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
SRC 5 ,6, 8 and 10 KVA ... Resolution : ... Do the SRC 5 -10 KVA ... turn on without battery when the Input ... ... taken out of service for maintenance) ... ... of the SRC 5 -10 KVA ... ... frequency, and battery voltage, etc ... ... /6/ 8 /10kvauxi Models ... ... 6A/ 8 A, in ... to keep the battery at full state ... thus extending the battery life. ... to choose a Service Bypass Panel? ... look into a service bypass panel which ...


Résultats 1 - 10 de 96

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.