Consulter la FAQ



Guidelines for installation of an acsc100, or acsc101
Guidelines for installation of an acsc100 ... Installation . Resolution : Guidelines for Installation ... self-contained cooling that maximizes availability ... ... reliability and rapid installation . For ... the InRow SC Installation manual (990 ... ... locations with seismic installation requirements, additional ... InRow SC Seismic Installation Manual addendum ( ... ... the influence of exterior heat loads. ... amount of fresh air for make up ... ... make-up air (if required ... The HVAC system must be capable of rejecting up to 34000 BTU/hr (10kw) of heat per unit. Refer to Application Note AN-109 and the InRow SC Installation manual for additional information.
How to navigate through an Network Air FM unit display
... through an Network Air FM unit display ... ... ACFM, Network Air , ir40. Resolution : ... FM DX Precision Air Conditioner. ... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... ... of the return air and the dew ... ... of the return air . ... of the room air . ... , then the cooling setpoint is used ... ... (PCIOMs) installed in the user ... Installation Air Filter. ... the type of air filters installed in the Modules ... ... recommended for typical installations . ... method used for heat rejection by the ... Air
What are your Cooling Product Energy efficiency rating (EER)?
... to calculate your Cooling Product Energy efficiency ... Install Resolution : ... heat pumps and air conditioners. ... of a particular cooling device is the ... cooling (in Btu ... ... using a 95F outside temp and an ... (actually return air ) temp of ... ... COP of a cooling device is unit ... less: the cooling load and the ... ... to Schneider Electric's cooling products this can ... This could be the expected return air temps or another value based on a competitors product rating point. ... = rated cooling capacity output (kW)/ cooling input power (kW) ... = rated heating capacity output (kW)/ heating input power (kW)
What are the typical uses for an EcoAisle System
... closely couples the cooling equipment to the IT heat load as it ... pressure inside vs outside the containment allowing ... right amount of air is being provided ...
Why does my InRow cooling unit keep alarming with warm start alarms
Resolution : ... the InRow RC air conditioner uses internal ... The InRow RC air conditioner implements internal watchdog mechanisms ... if the InRow RC air conditioner does not receive any network traffic for 9.5 ... Address Resolution Protocol [ARP] request), it assumes that there is a ... To ensure that the InRow RC air conditioner does not restart if the network is quiet for 9.5 minutes, the InRow RC air conditioner attempts to contact ... responds to the InRow RC air conditioner, and that response restarts the ... reset the 9.5-minute timer frequently enough to prevent the InRow RC air
Does the NetShelter VED Kit provide cooling?
... VED Kit provides cooling . ... choose the correct cooling option. Resolution : ... that the waste heat from the cabinet ... Servers and IT equipment have their own fans which force hot air to the back of the cabinet. If there is no larger AC unit drawing that hot air from the cabinet into the VED, then into the plenum, it might be advisable to incorporate an ARU (acf400, acf402) instead of a VED.
How to set up group communications for an Network Air FM unit
This article contains the step by step instructions on how to set up group communications in a Network Air FM unit. ... Network Air FM. ... Resolution : ... is an independent, Computer Room Air Conditioner. ... For more information on the dip switches set up, see the Installation Manual. ... 4.Please set the group configuration cooling load-sharing and System role-assignment functions ... If the environmental temperature or humidity is outside the range determined by the setpoint and threshold, the System will generate a load-sharing request.
Can I use Type L soft copper for my installation?
Can I use Type L soft copper for my installation ? ... All Air -Cooled Cooling Units ... DataCenter Room Cooling ... Resolution : ... Schneider Electric, requires all refrigerant installations to use clean, refrigerant-grade ACR Type L pipe, Hard Copper. It is expected all standard procedures are taken for pipe size selections for air -cooled equipment. ... In air conditioning applications or where pipes will be exposed, hard copper won't bend or sag under extreme heat . ... SOFT COPPER IS PROHIBITED AND IS NOT ACCEPTABLE. ALL INSTALLATIONS WITH SOFT COPPER WILL BE REJECTED.
Network Air FM unit spare parts list
Install Resolution : Please contact Cooling Tech Support to ... ... /Water & Air LL Filter Air 30% UF ... Filter Air 85% UF ... ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS O-RING 7/8" Teflon FM ( heat exhanger) ... PowerView Label Air (NOME) ... Air Miscellaneous Sku ... SEISMIC FLOORSTAND, 12" FM 35-50 KW W/ AIR DEFLECTORS ... SEISMIC FLOORSTAND, 18" FM 35-50 KW W/ AIR DEFLECTORS ... SEISMIC FLOORSTAND, 24" FM 35-50 KW W/ AIR DEFLECTORS
DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Resolution : Air Cooled Condenser Installation and Operating Instructions DAC Air Cooled Condensers For ... Cancoil air -cooled condensers ... , medium and high temperature refrigeration applications. ... equipment, proper installation and set- ... ... be used if air -cooled quipment ... ... cfm (of outside ventilation) per ... Installation Date __ ... Use high temperature silver solder or ... ... that will cause HEAT GAIN, it ... ... properly sized and installed to insure oil ... ... to minimize external heat gain and condensation ... ... risers should be installed with a trap ... Cancoil air -cooled condensers ...


Résultats 1 - 10 de 93

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.