Consulter la FAQ



CDU Spare Parts List
) 875-4342 Flange Dielectric Npt (Thread Piece ) 875-4344 Flexible Fluid Piping (100 Feet 30.4 Meters
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... Spare Part w0w3116 CDU Metric Pipe Connection ... ... W875-2014 Flexible Fluid Piping - ... ... Meters) acac20003 Flexible Fluid Piping - ... Meters) acac20002 Flexible Fluid Piping Clamp/Hanger acac20007 Flexible Fluid Piping Clamp ... 50) acac20008 Flexible Fluid Piping Couplings ... acac20006 Flexible Fluid Piping Couplings ... 875-4308 Flexible Fluid Piping Insulation - 100 Feet (30.4 Meters) acac20005 Flexible Fluid Piping Insulation - 300 Feet (91.4 Meters) acac20004 Flexible Fluid Piping Strut Mounted Clamp acac20009 FLOW METER - 1" (body of the flowmeter
How do I install Pex piping?
2. Runs from the CDU to the unit should be free of joints and bends should not exceed the suggested bend radius.
Uniflair Drain Line Connections
Connecting to the Drains The condensate water drains from the tray through a 1 1/4” flexible tube fitted in the unit .
What are some of the applications for the InRow ACRD?
... IT managers, facilities managers and contractors to install the same unit in different applications as a result of flexible heat rejection options like air ...
CDU Chilled Water Internal Volumes
ACFD12-T, ACFD12-B, internal unit volumes, internal volumes, water-cooled, gallons of water
CDU Installation Manual
Issue: CDU Installation Manual
ACFD12 Tech Data Manual
ACFD12-B, ACFD12-T, Tech Data Manual, CDU , Chilled Water, Distribution
Will the EcoAisle replace the tradition HACS offering
This flexible system adapts to both hot and cold aisles to address the wide range of data center cooling challenges faced by today's IT and ...


Résultats 1 - 10 de 32

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.