Consulter la FAQ



Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
Used Battery Disposal Options
If you purchased an APC Replacement Battery Cartridge in the ... to return the old battery will be provided with the new Replacement Battery Cartridge.
Safety Guidelines for Smart-UPS, BACK-UPS, and Surge products
, and only use official APC Replacement Battery Cartridges
Video: How do I troubleshoot the Replace Battery LED on a Smart-UPS?
The Replace Battery LED is lit ... The Replace Battery LED is designed ... illuminate when the battery needs to be ... ... troubleshoot your Replace Battery Indicator: ... . Allow the battery to charge to ... ... a minimum of 8 hours for a ... UPS with external batteries connected. ... products will charge batteries whether the unit ... ... If the Replace Battery LED remains lit, the battery needs to be ... Batteries typically last 3 ... can make the battery require replacement sooner. Battery contact APC Customer Support ... a possible warranty replacement , please . ... unit when contacting APC as additional troubleshooting ...
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... runtime remaining is 8 minutes or less , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... UPS battery ... /www. apc .com/ ... ... or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ...
Video: APC AV S Type Power Conditioner w/ Battery Back-up - Battery Replacement Procedure
Resolution: The following video details the process for removing and reinstalling the internal Replacement Battery Cartridge.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
How do I recycle APC batteries in the US and Canada?
Pack the used battery in the packaging from the replacement battery cartridge and affix the return label.
Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
Where can I get support for APC and MGE Products?
Battery Management Battery Replacement Services


Résultats 1 - 10 de 68

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.