Consultar las preguntas frecuentes

Galaxy VX; How to set up, stop or change the “Automatic Battery Test” option of the UPS

Fecha de publicación: 15 July 2020

Issue:
How to set up, stop or change the “Automatic Battery Test” option of the UPS



Product line:
Galaxy VX - all


Environment:
All


Cause:
How to set up, stop or adjust the Automatic battery test option


Resolution:
From the home screen on the display select Configuration > Battery > Test.



Set your preferred settings for the automatic battery test:

Battery Test Interval: Select your preferred interval for battery tests.
Choose between: Never, Every 52 Weeks, Every 26 Weeks, Every 12 Weeks, Every 8 Weeks, Every 4 weeks, Every 2 Weeks, or Once a Week.

NOTE: If you run battery tests too frequently it can reduce the lifetime of the batteries.

Battery Test Start Time: Select the time of the day in 24 hour format that
the test should take place and complete with Enter.

Battery Test Day of the Week: Select the day of the week that the test
should take place and complete with Enter.

When all settings have been completed, tap OK to confirm your settings.





 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.