Consultar las preguntas frecuentes

The “Generic Modbus” application does not provide status bits values in binary

Fecha de publicación: 27 December 2017

Issue:
The “Generic Modbus” application does not provide status bits values in binary

Product line:
Generic Modbus Application or Similar application


Environment:
Generic Modbus Application or Similar application


Cause:
The “Generic Modbus” application does not provide status bits values in binary


Resolution:
Take the value provided by the application and convert it to binary by using a calculate like the one provided by Windows.  If using the Windows calculator, you may have to change the calculator to scientific or Programmer mode to accomplish this conversion.

Below is a couple of examples from a Galaxy VX:

Example 1:  Register 400002 (16385)

16385 in BIN 100 000 0000 0001

This example has 14 bits and to get to 16 bits two zeros were added to the left (red text)

10 0000 0000 0001 is 0010 0000 0000 0001

 

Example 2:  Register 400010 (512)

512 in BIN 10 0000 0000

This example has 10 bits so six bits needs to be added to the left (red text)

10 0000 0000 is 000 0010 0000 0000




¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.