Consultar las preguntas frecuentes

Video: Data Center Operation | How to create logs if httpd service is down?

Fecha de publicación: 27 June 2019

Issue:
How to create logs if httpd service is down with StruxureWare Data Center Operation

Product Line:
StruxureWare Data Center Operation (DCO)

Environment:
StruxureWare Data Center Operation (All Versions)

Cause:
It is possible that during installation or upgrade that the Apache server (httpd) becomes unavailable. To be able to diagnose these types of concerns Technical Support would require the log files to determine a course of action.

Resolution:

 

Due to Apache (HTTPD) service being unavailable it is not possible to obtain log files via Webmin. Log files are about to be obtained via a console or SSL session using the following CLI command

1. Log into the Operation server via console or SSH.
2. Enter "cd /"
3. Enter " sudo   su "
4. Enter the password(this password is the same one used to access console/SSL)
5. Enter "Platform.pm collect-log-files / tmp " (this will create a log.tar.gz file located in the / tmp  directory)
6. Once the process is completed, FTP/SFTP the log file just created from the server to your PC.

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.