Consultar las preguntas frecuentes

"Battery Predicted Replacement Date" missing from AP9630/31 UPS Network Management Card 2 (NMC2) Web Interface on supported UPS models

Fecha de publicación: 25 September 2014


Issue

Certain UPS models that support "Predicted Battery Replacement Date" or "Battery Predicted Replacement Date" or "Next Battery Replacement Date" do not display the value in the installed UPS Network Management Card 2's web interface.






Product Line



  • UPS Device Management
    • UPS Network Management Card 2 (NMC2)
      • AP9630/30CH, AP9631/31CH

  • Smart-UPS models with the following model prefix
    • SMX
    • SMT

 

 
Environment
 

  • Supported UPS model listed above
  • NMC2 v6.2.0 sumx application firmware

Cause

This is due to a firmware bug.


Resolution

A future firmware revision will address this issue.

In the meantime, the value is available via the NMC2 Command Line Interface (CLI) via the detstatus -all command or via SNMP OID .iso.org.dod.internet.private.enterprises.apc.products.hardware.ups.upsBattery.upsAdvBattery.upsAdvBatteryRecommendedReplaceDate (.1.3.6.1.4.1.318.1.1.1.2.2.21).

Note: Support for the upsAdvBatteryRecommendedReplaceDate SNMP OID requires APC PowerNet MIB v4.0.8 or higher.



¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.