Consultar las preguntas frecuentes



Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
Please use acac10005 for 300 mm wide applications and acac10010 for 600 mm wide applications.
How to install InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010
Issue: InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide —acac100010.
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0 ...
Are 23" mounting rails available for NetShelter SX cabinets?
... : 23" wide mounting rails do not install into 600 mm (24") wide cabinets because the cabinets are not wide enough.
How many leak sensor cables can be attached in series on an 600 mm unit
Issue: This document answers the question of how many leak sensor cables can be attached in series on an 600 mm unit.
How do NetShelter SX cabinets bay together?
baying, bracket, 24in, 24 inch, 600mm, 600 mm ,
What is the exact placement of the cutouts on NetShelter SX mounting rails?
... , hole, holes, pma, 42u, 45u, 48u, 600 mm , 750 mm , 600mm, 750mm,
Can the NetShelter SX cabinets be bayed with the side panels on, and how do the baying brackets work?
There are two alignment holes on the bracket allowing the cabinets to be joined at 600 mm on center, or 24 inch on center ...
How to remove NetShelter SX rear doors when installed in rows.
When NetShelter SX cabinets are bayed at 600 mm , if the cabinets are not ... remove the right hand rear door from a cabinet.
50a 208v 3 Phase Rack PDU Load Ratings and Calculations Explained
Why is AP8868 rated at 10.0kw, when AP7868 was rated at 12.5kw? Previous generation rack PDUs, such ... .5kw rated rack PDUs. This ... UL did not de -rate the internal circuit breakers. Since


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.