Consultar las preguntas frecuentes



​Information for Noise level of UPS Galaxy 5000 NAM
UPS rating ( kVA ) 40 / 50 /60/80kva 100/130kva Noise level on a normal floor (dBA) with ...
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
... UPS VT- Galaxy 3500; Bypass ... ... UPS VT- Galaxy 3500-ais3000 ... the PFC is 40 Hz - 70hz ... a ) Mains distortion ... 60 HZ +/- 0, 1 % ... 50 Hz - 70 Hz For 50 Hz systems: 50 HZ +/- 0, 1 % ... 40 Hz - 60 Hz ... The phase difference between the output PLL and the bypass voltage is above a predefined limit and the system will not be able to go to bypass. ... When AC mains returns you may get a informational event for; Mains no longer prevents UPS from switching to bypass.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
The instructions to power down the UPS are available on the display. This procedure is for a single UPS with an external maintenance bypass panel.
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
The instructions to power down the UPS are available on the display. This procedure is for a single UPS without an external bypass panel.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000 , 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000 , 5000 and Galaxy PW ... , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or ... ... Monitoring Enclosure has a CB, power ... One is down ( ... ... Modbus card has a female DB9 so a male DB9 cable ... The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... Galax VX or Galaxy VM. Galaxy VX, Galaxy VM ... the password when first logging into a network device. ... display of the Galaxy VX and VM ... Use a terminal program with ... ... no parity, 1 stop bit, ... At this point you will be asked to enter a new password. ... Open a browser and enter IP Address; example address ... At the bottom of the screen you will a box to enter a password for “Pin [4-8 digits]” and a “Confirm Pin 4-8 digits]” and click on Save button.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be in a totally off state ... ... not for commissioning a new UPS. ... The commissioning of a new UPS must be performed by a Schneider Electric trained ... ... to restore the Galaxy 5000 UPS from ... ... procedure is for a single UPS without an ... Step 1 : Set the input Q 1 switch to On Step 2: Wait until the end of the UPS initialization with PFC start -up. ... Step 4: Choose “ Start the UPS” ... Step 9: Press the Green “Inverter Start Button”
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
1 .) Purchase a right angle DB25 Male-Female interconnection knowledge base article ID
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
The Galaxy VS internal NMC and the optional ... date and time which can cause a loop of trying to set the date and time.
Which modular batteries can be used with the Galaxy VS All in One (AIO) model?
It is not possible to program different batteries into a UPS.


Resultados 1 - 10 de 72

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.