Consultar las preguntas frecuentes



Symmetra PX 250/500 Battery to Power Module Ratio
The 250kw runtime ratio is 10 PMs to 16 battery shelves resulting in a ratio of 1.6 battery shelf per 1 PM. ...
Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
Symmetra PX1 20 - 80 kva, Symmetra PX2 100 kva, Symmetra PX 250 - 500 kva, SUVT, g3500, ais3000, ...
Can I install multiple APC SmartSlotAccessory Cards in one UPS?
Symmetra LX Symmetra PX (excluding PX 250 / 500 )
Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
... type APC modular batteries , and/ ... the SE modular batteries such as GVSBTU ... ... ,2, 250 - 500 , SUVT, ... ... and the PX 250 /500kva UPS units) batteries . Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. ... Galaxy VS Modular Batteries : Battery Type ... 1 .057 ... Battery Type ... 1 ... Battery Type
APC UPS Network Management Card (NMC) Compatibility Chart
Symmetra PX 250 / 500 ... Symmetra PX2 48kw All-in- One * Symmetra PX2 100/160 kW *
EcoBreeze Variable Speed Drive Technical Spec’s
Motor power kW 15 kW ... 200 V , 1 kA Speed range 1 ... ... ... AWG 14 L 1 , L2 ... ... Prospective line Isc 1 kA ... ... 500 Hz ... .m L 1 , L2 ... ... mA , impedance 250 Ohm ... V (state 1 ) LI1. ... ... V (state 1 ) ... configurable relay logic 1 NO + 1 NC , electrical ... ... switching current R 1 -R2 ...
NetBotz | Wireless Network Basics
... NetBotz 400- 500 Series ... NetBotz Rack Monitor 250 (nbrk0250) ... NetBotz Rack Monitor 250 , 400- 500 Series, 700 ... ... must have only one coordinator, which ... ... are powered by batteries . Choose one or more nbwc100us ... Connect one nbwc100u (USB ... ... : To preserve battery life, do ... ... to only turn ONE on at a ... Extending the coordintor above the rack level will provide better wireless single throughout the data center. ... For the NetBotz 250 , as simple USB extension cable (non-HUB) must be used.


Resultados 1 - 10 de 65

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.