Consultar las preguntas frecuentes



What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX; What ... maximum number of XR frames allowed with a Symmetra PX solution? Symmetra PX 20, ... ... maximum number of XR frames allowed with a Symmetra PX solution is 4 . ... size of the Symmetra PX Main Frame ... For a Symmetra PX 20 or ... number permitted is 4 fully populated (Battery Frames ) XR frames . ... a runtime of 1 hr 40 mins ... ... of addresses for XR frames . ... a fully populated XR frame is SYCFXR8 ... ... consists of the XR frame with 8 ... There are 4 Battery Units in ... this equals an XR frame with 32 ...
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
The XR frame of a single phase Symmetra displays E3 ... mainframe indicates an XR Frame Fault. Symmetra Power Array Symmetra RM Symmetra LX ... message on the Symmetra XR Frame is an ... communication between the Symmetra mainframe and the Symmetra Extended Run ( XR ) Battery Frame ... ... between the two frames where the Power ... located in the XR Frame. ... card on the Symmetra Extended Run Frame ... 1 ) Disconnect the ... back of the Symmetra Extended Run Battery ... 4 ) Reconnect the ... ... the E3 message should no longer be flashing on the XR Frame and on the PowerView ...
Single Phase Symmetra XR Frame Compatibility
Issue Single Phase Symmetra XR frames are compatible only with certain UPS systems.
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
Product Line Single Phase Symmetra XR Frames
Single Phase Symmetra XR Battery frame displays EF or E1
Symmetra LX Single Phase Symmetra XR Frames
Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500k PX is EPO'd
Symmetra PX ... describes how the Symmetra PX reacts to ... ... , from a single point by activating ... ... circuit in the Symmetra PX is activated ... or in the XR Frame (80kw ... Mains feed CB will be tripped on ISX PDU . There is no power on the output of the XR Battery Frames or on the output of the Symmetra PX UPS. ... Only the Battery CBs on XR frames will be tripped. ... All Battery CBs on battery frames and Q2 will be tripped
Batteries discharged to a low voltage in a single phase Symmetra frame
... discharged battery modules installed in the system (this includes any battery modules in connected XR frames ).
Mounting the Symmetra LX in a 2 post rack
How do I mount a Symmetra LX in a 2 post rack? ... Symmetra LX ... Symmetra LX ships with a 4 post rail kit only, however it is possible to safely mount the UPS system and any associated XR frames in a 2 post rack. ... ( 1 ) SYOPT12 must be purchased and used for each Symmetra LX mainframe or extended run ( XR ) battery frame that is to be mounted.
Symmetra Power Array reads "Bypass Out of Range"
Symmetra Power Array shows ... Symmetra Power Array ... This document describes one of the reasons ... a North American Symmetra Power Array may ... ... operation of a Symmetra Power Array, ... ... default, the Symmetra Power Array comes ... ... input of the Symmetra to a 240vac ... ... " of the Symmetra Main Intelligence Module ... ... (0's or 1's ). ... indicates whether the Symmetra's Input Voltage Jumper ... ... equal to " 1 ", then ... ... refer to chapter 4 in their Symmetra User's Manual. 1 . Turn the ... ... rear of the Symmetra . ... front of the Symmetra . 4 . Open the ... 6. Disconnect any extended run ( XR ) battery frames , if applicable.
How to change the Input Voltage Select Jumper on a Symmetra Power Array
I have changed the operating environment of my Symmetra Power Array and need to change the input voltage setting; what is the proper procedure? ... Symmetra Power Array ... 1 . Switch the System Enable switch to the OFF position. ... 4 . Remove all battery modules from the UPS. 5. Disconnect any extended run ( XR ) battery frames from the UPS. ... 1 . Refer to figure below.


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.