Consultar las preguntas frecuentes



Video: Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware
... perform or complete a firmware upgrade on ... Firmware revisions 5 . X . X , 6. X . X . ... device from v 5 . X . X to v6. X . X , please review ... ... the BIOS in a computer system. ... it by using a serial communications cable ... ... relevant commands ( a full list of ... available in Appendix A at the end ... ... Steps 4 - 5 ) and how ... ... be used if a serial port is ... In a terminal emulator application (for example ... Data bits 8 ... and may take a few attempts to ...
ACSC1XX Spare Parts List
Manufacturing # ... BRACKET SCREW M 5 X 12 FLT UCUT PHIL M 5 X 12 BLK ( ... ... MTL PPR 400v 5 % 40uf RD ... ... Ceiling Tile Adapter 24 " - Spare ... ... .13" X .13" X .13" ... .19" X .19" X .19" ... DIVIDER-' A ' DUCT KIT ... DUCTING KIT 24 INCH IR5 ... , 3/ 8 " ODF ( ... ... FITTING 1/ 8 " BARB 10 ... ... FITTING 1/ 8 " BARB TEE ... ... DRIER 3/ 8 "ODF SOLDER
Network Air FM unit spare parts list
... "-12R 7 / 8 "SWT ... "-14R 7 / 8 "SWT ( ... ASSEMBLY FLOW RATER FM ... ASSEMBLY FLOW RATER FM ... ASSEMBLY FLOW RATER FM ... A 9-30 ... Door Handle Assembly (old handle ... ... UF & DF 5 /Unit 756 X 325 X 102mm (29.7 X 12.8 X 4IN) ... UF & DF 5 /Unit 756 X 325 X 102mm (29.7 X 12.8 X 4IN) FLOORSTAND 24 " FM35- ... ... CLASS CC 3 A 600vac ... CLASS CC 6 A 600vac
Video: Data Center Expert | Backing up to a Windows Share
... Process for creating a Windows share backup ... ... version 6. X to 7 . X ) ... be performed on a regular basis. Creating a Windows Share Performing a Backup within DCE Creating a Windows Share ... versions may prevent a windows share from ... ... 1) Create a folder on the ... 5 ) Set the ... 7 ) Select Advanced ... 8 ) Ensure that ... ... user as step 5 ). Performing a Backup within DCE ... Steps 3 & 5 ) ... computer is on a domain, enter ... ... Subdirectory: If a subdirectory was created ... 5 ) Select Test ... 7 ) Select the ...
NetBotz 750 | Resetting a Lost Root Account Password
NetBotz version 5 NetBotz v 5 . X Reset a Lost Root Account ... ... 1) Connect a USB- A to Micro USB ... NetBotz appliance and a USB port on ... ... 2) Open a serial connection on ... ... Data Bits: 8 ... use by another application . ... do not press a key within five seconds after you ... 5 ) Enter the ... 7 ) Disconnect and ... ... do not press a key within 5 seconds after you ... 8 ) Enter the following three commands: ... NOTE: If you do not complete steps 7 and 8 , the root password will be reset every time the appliance restarts.
PowerChute Network Shutdown lost communications or cannot establish communication with UPS.
... running The most current version of PowerChute ... ... .2. X and below. ... #ifconfig - a " to display ... ... PCNS 3. X and above can ... PCNS and registration now occurs post installation ... 5 . Verify that the PCNS service is started. ... stopping the PCNS service can be found ... 7 . PowerChute Network ... lease and acquires a different IP address ... have a permanent IP address ... ... should also have a static IP address ... 8 . If the system is on a different network segment ... (See Application note PowerChute Network ...
Network Management Card (NMC) Password Reset Procedure
... lost and requires a special reset procedure ... Connecting a non-APC ... ... trying to reset a password on a UPS that has ... Select a serial port at ... and disable any service that uses that ... ... UPS devices with a DB-9 ... Run a terminal program (such as ... ... UPS devices with a DB-9 ... ... 2400 bps, 8 data bits, ... ... 9600 bps, 8 data bits, ... ... 200 bps, 8 data bits, ... ... 9600 bps, 8 data bits, ... ... 9600 bps, 8 data bits, ... ... 9600 bps, 8 data bits, ...
INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
... To verify your current firmware version: ... for AOS and APP : ... v6. X . X firmware has an ... ... this is v 5 . X . X firmware and is ... ... firmware, try a reboot first. ... roughly equivalent to a Basic Input Output ... BIOS) of a computer or device ... a computer that supports a terminal emulation program (If a firmware upgrade is ... your terminal emulation program must support XMODEM ... Select a serial port at ... and disable any service that uses the ... Run a terminal program such as HyperTerminal ... 57600 bps, 8 data bits, ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
You have a device such as a Rack PDU, ... You had a problem with a previous upgrade attempt ... ... with the wrong application and you need ... load the correct application . ... Also, sometimes a firmware upgrade can ... ... device from v 5 . X . X to v6. X . X , please review ... ... pertain to your application . ... multiple devices at a time, ... AP9635 installed in a Symmetra PX 250 ... , you have a Network Management Card ... ... Card installed in a UPS, you ... ... /tools/ software -firmware ... Filter by > Software / Firmware
Video: How do I configure APC Network Management Card network settings?
A Network Management Card ... being accessible via a network. ... (such as a AP78XX or AP79XX ... ... are configured for a boot mode of ... ... using DHCP, a vendor cookie ( ... ... APC devices have a MAC address that ... C0 B 7 ... Configuration Wizard is a Windows application designed specifically to ... ... version 3. x . x or higher. ... NMC can obtain a DHCP address and ... ... C0 B 7 , which indicates ... ... settings will have a solid green status ... ... be to use a direct network connection between a computer and the ... ... will be on a peer to peer ...


Resultados 1 - 10 de 65

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.