Consultar las preguntas frecuentes



Single Phase Symmetra Battery Capacity Below 100%
... time to charge its batteries but is ... showing a battery capacity value below 99% or 100 %, there ... battery modules in its frame.
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
1 ) ... be able to support the load attached ... ... the battery is 100 % charged, ... ... once every 6 months while in storage ... ... be plugged into it . ... is capable of supporting a load of ... ... you're trying to support , please use ... ... printer connected to it . The computer ... A single piece of equipment ... If one input cord is ... ... a UPS on one input and Utility ... It will begin with ... ... UPS thus causing it to shutdown and ... ... to battery, it may have an ... ... very uncommon with IT equipment. ... type of connection it is important to ... Each UPS must have its ' own pair of wires running back to the EPO switch.
Why are the battery charge LEDs flashing on a Smart-UPS?
Option 1 : ... battery is at 100 % capacity . Sometimes it is necessary to ... ... cut power to its , therefore, ... battery by disconnecting it from utility power ... ... on battery until it turns off completely ... ... outlet and allow it to recharge ( it will recharge more ... ... contact APC Customer Support ... UPS and on its battery capacity . ... , 80, 100 % (bottom ... ... factors, battery capacity and UPS load ... When utility power is lost, the UPS begins discharging the battery in order to support the attached load. Once power returns, the Smart-UPS will automatically begin to recharge its battery.
Battery Discharge During Storage
At 20° Celsius, a battery will lose 3% of its capacity per month .
SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS. How do I update it?
... SmartConnect enabled ( EcoStruxure ™ Ready) ... EcoStruxure ™ Ready Smart ... EcoStruxure ™ Ready Smart-UPS products are able to download the latest UPS Firmware from the Cloud. ... https://www.smartconnect- support .apc.com/help/EN/index.html#page/ EcoStruxure %2520ready%2520smart-UPS%2520help%2520center%2fmn04.6.2.html%23 ... 1 - To upgrade the firmware you can do so via the cloud portal.
Data Center Expert | What virtualization environments are supported?
... virtualization environments are supported for the Data ... ... recent information on supported virtualization platforms can ... found within the EcoStruxure IT Help Center at ... ... virtual appliance, supported on VMware ESXi ... ... device nodes and one surveillance node. ... nodes and activate supported applications, or ... ... is the first supported virtualization platform. The Data Center Expert virtual appliance is delivered as an OVA (Open Virtualization Archive), expected to function properly on any virtualization platform that supports this format, or has an appropriate converter utility. ... There is currently no planned support for any other virtualization platforms, including Microsoft Hyper-V.
Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
How to Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003 ... Native serial shutdown is not supported with Smart-UPS model family SMT, SMX, ... Step # 1 : ... Note 1 : ... 1 Stop Bit ... UPS, you will also receive information such as Runtime, Battery Capacity and battery condition. ... If hibernation is not enabled, there will be no hibernation tab and it will not be listed in shutdown ... If this is the case, your BIOS may not support hibernation or it may be disabled.
What are the supported port speeds for the APC Network Management Card and network enabled devices?
Supported Ethernet network port ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... APC Network Management Card 1 and 2 enabled products can be set to one of the following settings in terms of Ethernet port speed: ... 100 Half-Duplex 100 Full-Duplex ... If the card has difficulty in negotiating a speed with the network switch, it will choose 10 Half-Duplex. ... Some switches may support 1000/100mbps and will auto-negotiatiate. ... Other switches support 10/100mbps modules/add-ons for connectivity.
What is Modbus and How does it work?
What is it used for? ... , meaning that it's free for manufacturers ... It has become a ... It is used widely ... How does it work? ... would be a single serial cable connecting ... ... as series of ones and zeroes called ... ... voltages and a ones as negative. ... troubleshooting problems, it can be helpful ... ... Long strings of ones and zeroes are ... ... is represented by one of the sixteen ... is represented by one of the 256 ... ... or contact is 1 bit and assigned ... ... Each register is 1 word = 16 ... 1 , 10001, ...
Data Center Expert | How do hardware and software support contracts work?
... warranty and software support contracts work for ... Software Support Contract software support . ... and complete software support in order to receive technical support and software upgrades ... Software support contracts are required ... under base software support SKUs) as ... ... not currently require support contracts. Hardware Support Contracts Hardware support must be continuous ... Year 1 ... Out of HW Support ap9470 Factory Factory ... Out of HW Support AP9475 Factory Factory ... Out of HW Support Software Support Contracts Software support can not be ... virtual appliance until it is activated using ... Support contracts start at ... ... systems, the support will begin when ...


Resultados 1 - 10 de 80

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.