Consultar las preguntas frecuentes



Why won't my Lithium-Ion Smart-UPS start when the battery is first connected when there is no utility power to the unit?
... then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start .
Frequently Asked Questions for the new Lithium-ion Smart-UPS products.
The UPS has a unique internal battery connector to avoid any misconfigurations in the field.
How to Cold Start a Symmetra LX Extended Run Frame
The extended run frame needs to have at least one good battery installed with the black knob on the front of the battery in the ...
How can I adjust the number of battery packs on a Smart-UPS XL?
1 . First , EXIT out of the PowerChute plus Server. In the case of Windows NT,
Adding External Batteries to an SU, SUM, SURT, SURTA, SURTD or SUA series Smart-UPS XL
... to set your unit to ""0"", the first external battery would be "" 1 "".
Matrix UPS will not perform a runtime calibration
1 . Battery capacity must be 100% at start of calibration (all packs must indicated as float).
Why is my UPS emitting a single beep every few mins?
... customer when the UPS has sensed a power anomoly and has begun to power the connected equipment from it's internal batteries .
Matrix-UPS emits a chirping sound after being on-battery or running a self-test
... If a SmartCell battery pack fails a UPS On- Battery Self-test ... or through UPS start -up) ... an interval of one minute to warn of a Replace Battery condition.
PowerChute Network Shutdown continually shuts down the ESXi host following On Battery Shutdown and UPS turn off when A/C power has been restored in Advanced UPS Configuration.
1 . To prevent the ESXi hosts from being continually shut down, re- start the PowerChute Network Shutdown service using the Windows Services ...
What does the Force Negotiation setting achieve in the Network Management Card?
starts with the NMC Low Battery Duration value, ... , if the battery duration time is ... values in # 1 and #2 below to ...


Resultados 1 - 10 de 95

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.