Consulter la FAQ

Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?

Date de publication : 20 February 2020

Issue:
Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.

Product Line:
NetShelter SX

Environment:
AR7721, AR7722, AR7723

Cause:
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.

Resolution:
The vertical cable manager can be installed in the rear-most facing position so that a PDU can be mounted behind it.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.