FAQs Techniques

Poser une question

Filtre de Résultat

    Rating and Use of UL489 Molded Case Circuit Breakers in APC Rack Power Distribution Products
    While there are some circuit breakers that are Listed and marked for 100 % use, circuit ... of these circuit breakers in Rack PDUs.
    How do software support contracts work for StruxureWare Data Center Expert.
    ... have an AP9465 StruxureWare Data Central Basic with an additional 100 node license and you want them to be under support for a year, ...
    Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
    Rack Power Distribution Unit ... Rack Automatic Transfer Switch ... ... policy is provided for reference or documentation ... APC will continue to honor the product warranty on a Rack PDU or Rack ATS if a licensed electrician is used to change the input plug or provided the replacement plug has the equivalent ratings of the original APC supplied plug. ... For more information on UL markings, please see the attached document. ... APC Rack ATS and Rack PDU products have not been evaluated by safety agencies for hardwiring in the field and as such, customer modification of these products for hard wiring cannot be supported.
    Register Map For NetBotz 200 and 250 does not include external sensor pod sensors.
    Register Map For NetBotz 200 and ... ... the modbus output for the sensors connected ... SNMP output will work fine for these sensors and if using StruxureWare DCE, you can use it's modbus output capabilities (with the AP95MODBUS license ) to output the sensor pods for the 200 and 250. The 250, beginning with AOS v6.5.0/nb250 v6.5.0, now includes support for remote sensors, external sensor pods, rack access, and wireless sensors.
    Power Specifications for NetBotz Version 1 Appliances
    Power Specifications for NetBotz Version 1 Appliances ... Power Specifications for Version 1 Appliances : -The electrical specifications listed below for the all of the units 303, 310 and 400 (Wall and Rack units). ... -Input Voltage (US power supply) : 100 - 240 VAC
    What are the supported port speeds for the APC Network Management Card and network enabled devices?
    ... network port speeds for APC Network Management ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... 100 Half-Duplex 100 Full-Duplex ... Other switches support 10/100mbps modules/add-ons for connectivity.
    INFORMATION BULLETIN - Using Global Outlet Groups simultaneously between AP79XX and AP8XXX series Rack PDUs with the same multicast IP range causes AP79XX PDU not to boot properly
    ... All Rights Reserved Rack PDU APP v ... Rack Power Distribution AP79XX Switched Rack PDU AP89XX Switched Rack PDU 2G ... AP79XX series Switched Rack PDUs. ... met in order for the issue to ... ... generations of Switched Rack PDU are enabled ... ... groups of Switched Rack PDUs are utilizing ... ... groups of Switched Rack PDUs are on ... ... generations of Switched Rack PDU active in ... ( For example, similar ... different generation of Rack PDU to your ... ... the AP79XX series Rack PDU which will ... ... Multicast IP range for each series of Rack PDU, and ... ... section, look for the following values ...
    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... For users upgrading ( ... For example, if ... For example, if ... ... X firmware executable for Smart UPS and ... ... X firmware executable for Smart UPS w ... ... The correct firmware for each platform must ... ... has been discontinued for some time and firmware for this device is ... ... the appropriate application for your type of ... ... upload the firmware for each device. ... that works best for you.
    SNMP OIDs Required for Rack PDU 2G Products (AP86XX, AP88XX, AP89XX)
    Issue: SNMP OIDs required for Rack PDU 2G products - which are correct?
    Can the ends of a NetShelter 2-post or 4-post rack be closed with panels?
    Issue: The customer wants to close off the ends of their open rack for a clean look.
    Résultats 1 - 10 de 90