FAQs Techniques

Poser une question

Filtre de Résultat

    What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
    The NetShelter CX also uses a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate (HPL) on its top ...
    How do I upgrade and activate premium devices in StruxureOn?
    About Premium You can upgrade the devices that are critical for your business to ensure you get expert assistance for monitoring those devices closely in case critical alarms. ... 24 /7 expert monitoring of your data center
    How to install a Remote On/Off (EPO) in a Uniflair unit.
    ... 4.1 24 Vac digital inputs ... inputs can be 24 Vac. The following figure represents one of the most common diagrams for connecting the 24 Vac digital inputs, for a pco3. ... 4.h and 4.i show the connection diagrams for the versions: MEDIUM (extended) and LARGE (limited to the part regarding the terminals located inside, on the board). ... The input contact will utilize the 24 volts from the units control transformer the exteral switch will be a dry contact to which will control the function or unit operation.
    What are the operational conditions for an InRoom (Stulz) Unit
    Return air conditions for evaporator capacity (DX): 24 °C (75°F) 50% R. H. Return air conditions for cooling capacity (CW): 24 °C (75°F) 50% R.H. ... Chilled water medium (CW): 0% Glycol
    Video: Data Center Expert | Managing Users
    , which is the full path to bind user within the authentication server structure . ... Users can no longer log into DCE after changing Active Directory or OpenLDAP structure . - DCE records the specific structure of the authentication server search base. ... - If the server cannot be brought back online with the same IP or server name, contact your local technical support for assistance .
    Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
    There are two ways to calibrate the unit with help of these menus: ... If the outlet load reads 2.4 amps without load then provide the value as '- 24 '.
    NetBotz Rack Access PX - HID (AP9361) | How do I configure RADIUS authentication for my card reader?
    client 159.215.4.0/ 24 ... If you have trouble configuring your RADIUS server, it is advised that you contact your RADIUS server vendor for assistance .
    Which NetShelter cabinets are compatible with EcoAisle and HyperPod?
    Issue: Not all NetShelter cabinets can install into both EcoAisle and HyperPod .
    Résultats 1 - 10 de 87