Consulter la FAQ



Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... of new Galax VX or Galaxy VM. Galaxy VX , Galaxy VM ... The display of the Galaxy VX and VM is part of the NMC and has been disabled. Resolution : ... Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... At the bottom of the screen you will a box to enter a password for “Pin [4- 8 digits]” and a “Confirm Pin 4- 8 digits]” and click on Save button.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS Resolution : ... This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 5 : Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch. ... Step 8 : Unlock CB2, remove the key, and place it in the key interlock. ... Turn off Q 1 Switch
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power off to normal on-line operation. ... Galaxy 5000, Galaxy 5500 ... For various reasons, the Galaxy 5000 may be in a totally off state. ... Resolution : ... How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On ... Step 5 : Turn the Q4S Switch to On ... Step 8 : Set the battery circuit breaker(s) QF1 to the On Position.
Galaxy VX; Customer, consultant or engineer looking for the center of gravity (CoG) for the IO and/or PC enclosures
Galaxy VX ... Resolution : ... GVX PC: X -distance 290mm, Y-distance 930mm , Z-distance 440mm GVX 750kw IOC: X -distance 590mm, Y-distance 830mm, Z-distance 390mm GVX 1000kw IOC: X -distance 590mm, Y-distance 830mm, Z-distance 390mm GVX 1500kw IOC: X -distance 1060mm, Y-distance 970mm, Z-distance 430mm gvxmbcr750: X -distance 399.7mm, Y-distance 993mm, Z-distance 471.5mm ( X =width, Y=height, Z=depth)
Information regarding the Aluminum cable for the Galaxy VX products
Information regarding the Aluminum cable for the Galaxy VX products. ... All Galaxy VX 1250 KW, 1500kw ... Resolution :
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX ? ... Galaxy VX ... How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX ? Resolution : http://www.apcmedia.com/salestools/MBPN-A35JB8/MBPN-A35JB8_R 1 _EN.pdf?sdirect=true See illustration below and link to Installation manual ... This should be left up to the engineer of record for the installation .
Galaxy VX; How to configure the Network Communications options
How to configure the Network Communications options for Galaxy VX ... Galaxy VX - all ... Resolution : The network can be configured for the display and for the cards in Smart Slot 1 and ... Smart Slot 1
Galaxy VX; What is the Airflow and BTU heat dissipation?
FSRs and or TSE members are asked for the Airflow and BTU / heat dissipation of the Galaxy VX product. ... Galaxy VX ... Air Flow information is not included in the Technical Specification or Installation documentation. BTU/hr information is present in the Technical Specification and Installation documentation. Resolution : This table is the estimated airflow in m^3/hr and CFM for the same four load level (three at 30c and one at 40c) as the heat dissipation (BTU/hr) tables found in the documentation.
Where can I find Modbus Register map for Galaxy VX UPS products
... map, Modbus Installation , Modbus Troubleshooting, Galaxy VX with Modbus, ... mod-bus installation , GVX use ... Modbus Modbus, Galaxy VX Modbus ​


Résultats 1 - 10 de 53

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.