FAQs Techniques

Poser une question

Filtre de Résultat

    Water leak in DataCenter.
    ... you find a Water leak on Indoor ... All DataCenter Cooling Units. Resolution : ... from coil to outside or to sewer ... ... Heavy particles will settle to the bottom ... ... , flush with water , or blow air through it to ... ... pour scalding hot water into it. An air trap will sooner ... ... side of the air flow, it ... a trap or air /gasses may ... ... also cause the water to back- ... ... it may run water from nearly any ... ... , restriction of air flow, be ... clogs may cause the condensation water from the air conditioner to back up and overflow. Use the hot water tip above to clear it.
    How to navigate through an Network Air FM unit display
    ... through an Network Air FM unit display ... ... ACFM, Network Air , ir40. Resolution : ... FM DX Precision Air Conditioner. ... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... ... ® (chilled water ) and DX ... ... of the return air and the dew ... ... of the return air . ... of the room air . ... , then the cooling setpoint is used ... ... (PCIOMs) installed in the user ... Installation Air Filter. ... the type of air filters installed in the Modules ... ... recommended for typical installations . Air Water
    What does water collection pan full mean and how do I fix it?
    What does water collection pan full ... Data Center Cooling Resolution : "The Water Collection Pan alarm ... is full of water . ... drain line or air bubbles. ... downward as the water exiting the condensate ... be submerged in water ). ... line inside or outside the unit, ... to clear the water pan full alarm ... If the unit goes in and out of the alarm state that would be different, but if one water pan full alarm lasts for an hour or more the condensate pump inside should be inspected.
    APC Schneider Cooling Unit Identification
    APC Cooling Unit identification. All Cooling Units. Resolution : FM Air / Water /Glycol Air Pattern ... Expansion A= Air Cooled E= Air Cooled W= Water Cooled F= Water Cooled D= Water Cooled ... W= Hot Water Air Pattern ... C= Chilled Water Air Pattern ... C= Chilled Water Air Pattern ... C= Chilled Water Air Pattern ... Main A= Air Cooled W= Water Cooled Air Pattern ... ) A= Air Cooled W= Water Cooled Air Pattern ... ) A= Air Cooled W= Water Cooled Air Pattern
    How to clean Air Filters on an acrc301s or acrc301h
    Component Replacement Air Filters. ... Install , Repair. Resolution Safety information before working on any Schneider Electric Cooling Unit Before You Start Powering down the unit, To stop the cooling unit Cleanable Air Filters Removal and installation 1. Starting with the top air filter, locate the pull tab and pull up and away from filter track. ... 3. Remove dust and debris from the filter media using a vacuum with a soft brush, or rinse the filter media with low pressure water . ... Make sure the filter is dry before installing .
    Network Air FM unit spare parts list
    Network Air FM unit spare ... Install Resolution : Please contact Cooling Tech Support to ... ... 4183 Glycol/ Water LL ... 4182 Glycol/ Water & Air LL Filter Air 30% UF ... Filter Air 85% UF ... ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... FM NAM 35KW WATER , R22 ... FM NAM 40kw WATER , R22 ... FM NAM 50kw WATER , R22 PowerView Label Air (NOME) Air Miscellaneous Sku Rope Water Detector Assembly ( ... ... KW W/ AIR DEFLECTORS
    What are your Cooling Product Energy efficiency rating (EER)?
    ... What are your Cooling Product Energy efficiency ... Install Resolution : ... heat pumps and air conditioners. ... of a particular cooling device is the ... cooling (in Btu ... ... using a 95F outside temp and an ... (actually return air ) temp of ... ... COP of a cooling device is unit ... less: the cooling load and the ... In regards to Schneider Electric's cooling products this can be calculated from the Technical Data Manuals, or Technical Data Specifications. ... This could be the expected return air temps or another value based on a competitors product rating point. ... = rated cooling capacity output (kW)/ cooling input power (kW)
    Guidelines for installation of an acsc100, or acsc101
    Guidelines for installation of an acsc100 ... Installation . Resolution : Guidelines for Installation ... self-contained cooling that maximizes availability ... ... reliability and rapid installation . For ... the InRow SC Installation manual (990 ... ... locations with seismic installation requirements, additional ... InRow SC Seismic Installation Manual addendum ( ... ... the influence of exterior heat loads. ... amount of fresh air for make up ... ... make-up air (if required ... Refer to Application Note AN-109 and the InRow SC Installation manual for additional information.
    How to set up group communications for an Network Air FM unit
    How to set up group communications in a Network Air FM unit. ... Network Air FM. ... Resolution : ... is an independent, Computer Room Air Conditioner. ... For more information on the dip switches set up, see the Installation Manual. ... 4.Please set the group configuration cooling load-sharing and System role-assignment functions ... If the environmental temperature or humidity is outside the range determined by the setpoint and threshold, the System will generate a load-sharing request.
    High Supply Temp Shutdown Installation on a NetworkAIR FM
    High Supply Temp Shutdown Installation on a NetworkAIR FM ... Data Center Cooling ... Resolution : ... Output contacts can map internal alarms and events to outside devices. ... These are the settings that will shut down the air conditioner. ... Set the low threshold very low and the high above the cooling Setpoint plus the deadband and a exaggerated factor.
    Résultats 1 - 10 de 90