FAQs Techniques

Poser une question

Filtre de Résultat

    How to install InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010
    Issue: InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010.
    Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
    The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0 ...
    How to remove NetShelter SX rear doors when installed in rows.
    When NetShelter SX cabinets are bayed at 600 mm , if the cabinets are not leveled correctly it may be difficult to remove the right ...
    How do NetShelter SX cabinets bay together?
    baying, bracket, 24in, 24 inch, 600mm, 600 mm ,
    What is the exact placement of the cutouts on NetShelter SX mounting rails?
    ... , hole, holes, pma, 42u, 45u, 48u, 600 mm , 750 mm , 600mm, 750mm,
    Are 23" mounting rails available for NetShelter SX cabinets?
    Compatibility Note: 23" wide mounting rails do not install into 600 mm (24") wide cabinets because the cabinets are not ...
    Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
    There are no square holes in the roof of the 300 mm chilled water cooling units so there's nowhere to connect the tabs on the NetShelter cable partition. ... Please use acac10005 for 300 mm wide applications and acac10010 for 600 mm wide applications. ... NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof. See the installation manual of the NetShelter trough, instruction # 2 . ... The mounting tabs on the bottom of the bottom of the 300 mm wide trough may be bent out of the way if there are no mounting holes.
    Can the NetShelter SX cabinets be bayed with the side panels on, and how do the baying brackets work?
    There are two alignment holes on the bracket allowing the cabinets to be joined at 600 mm on center, or 24 inch on center ...
    How many leak sensor cables can be attached in series on an 600 mm unit
    1 . Connect the leak sensor to the equipment using the plug located as shown.
    Where can I get support for APC and MGE Products?
    ... 6 0034- 1 0034-100 ... 100 0035- 2 M -E 0035 ... 0035-3 M -E 0035nd- 2 M - 1 E 0035nd-3 M - 1 E 0039- ... ... 25 0088- 2 M -E 0088-3 M -E 0088 ... 50 0088nd- 2 M - 1 E 0088nd-3 M - 1 E 0100-6RA 0129- 2 M -E 0129nd- 2 M - 1 E 0226- ... 3 0377- 1 M 0377- 2 M 0377-3 M 0386-
    Résultats 1 - 10 de 58