FAQs Techniques

Poser une question

Filtre de Résultat

    Can EPO Circuits be Wired in Parallel?
    Independant poles of an EPO (single action, multi-pole) switch must be run to each UPS.
    acpa4000 Spare Parts List
    w0h-0213 WIRE HARNESS 10 " SMART-SLOT (connects NMC to the brain board 0w0436 Services Description:
    Universal Transfer Switch (UTS) – FAQ
    Why does the uts10bi have two 10 awg Neutral wires ?
    NetBotz 455 | Physical Description
    Provides communications and power to the connected devices over standard CAT-5 cabling with straight-through wiring . 4 10 /100 Base-T network port Provides for a 10 /100 Base-T network connection and power through Power-over-Ethernet (PoE).
    SurgeArrest - minimum install distance of 10 meters (30ft).
    Do not install this device if there is not at least 10 meters (30 feet) or more of wire between the electrical outlet ...
    What are the differences between the Back-UPS RS and the Back-UPS XS models (Does not Include BX/BR LCD Models)
    ... line 2- wire phone/fax ... line protection and 10 /100base- ... line 2- wire phone/fax/modem protection.
    NetBotz 750 | What parts come with the NetBotz 750?
    ... to IEC-320-C14 power cord , 1. ... ft) 1 10 NEMA 5- ... -C13 power cord , 1. ...
    Password Reset on a V3 NetBotz appliance
    2. Using a thin wire such as a paperclip, press and hold down the reset switch for ten seconds. This
    Can you hardwire the input/output of the Matrix-UPS?
    A user may wish to hardwire the input/output of the UPS rather than use the supplied input power cord . ... These hardwire kits replace the standard back plate and allows the input and output of the Matrix to be wired directly to their corresponding electrical panels. ... Input/Output Wire Size ... 5kva: 10 AWG
    Résultats 1 - 10 de 86