FAQs Techniques

Poser une question

Filtre de Résultat

    Is there a baying kit or bracket to connect a NetShelter SX to a VX?
    Issue: Customer has SX and VX cabinets installed side by side.
    Are the NetShelter SX and VX cabinets Zone 4 compliant, high seismic, IBC or NEBS?
    Issue: Customers need to understand the seismic ratings of NetShelter SX and VX Seismic cabinets.
    Can split doors be installed on the front of a NetShelter SX, VX or SV cabinet?
    Resolution : Rear split doors can be installed onto the front of a NetShelter SX , VX and SV cabinets.
    Where are the Model and Serial numbers on the NetShelter SX, SV or VX?
    serial number, location, sx , vx , vl, av, colo, number, model number, sku number, sku
    What spare parts are available for my NetShelter SX, VX, WX, AV, SV, Colocation, EP, ES, VS, 2-Post Rack, 4-Post Rack?
    ... key, nut, bracket, paint, ground, key, hinge, sx , vx , sv, wx, es, ep ...
    Why are the Dell ReadyRails II loose?
    Product Line: NetShelter SX , VX , SV, CX
    Can the NetShelter SV be joined with other ISX Row Based components (InRow Cooling, UPS, PDUs)?
    ... to the different height, depth and frame design of the NetShelter SV, SX and VX cabinets.
    Are baying brackets available for NetShelter SX to VX?
    Issue: Customers may be looking for baying brackets to connect SX cabinets to VX cabinets.
    Résultats 1 - 10 de 55