Consulter la FAQ



Data Center Expert | Trial version VM appears to have 25 nodes available.
This is by design. It was done so APC did not need to add a 5 node key to just this one version.
Data Center Expert | How do hardware and software support contracts work?
... come with 2 years of factory hardware ... ... has a default 25 nodes (covered under ... as each additional node license. ... a total of 5 years , which includes 2 years of factory warranty ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 ... virtual appliance until it is activated using ... ... amount of Device Nodes Installed ... all of the Node Count (column ... ... covers the base 25 nodes installed on the ... 1 Year Software Support SKU 3 Year Software Support SKU
PowerChute Business Edition Agent fails to connect using simple signaling on RHEL 5.x due to SELinux access policy
OS: Red Hat Enterprise Linux (RHEL) 5 .x x64, x86 Build: PowerChute Business Edition 9.1.1 and 9.0.3 OEM Basic and 25 Node Deluxe ... The policy forbids a library used by the PowerChute Agent from running in its current context.
Where can I view community resources and documentation for Data Center Operation?
... .exchange.se.com/t 5 / EcoStruxure - IT -forum/bd-p/ ecostruxure - it -forum
Data Center Expert | What virtualization environments are supported?
The most recent information on supported virtualization platforms can be found within the EcoStruxure IT Help Center at: ... The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate from a server hardware version to a virtual appliance.
Runtime Calibration feature requirements for SMX/SMT units
... working properly, it is either refused ... ... one XBP: 25 %; with ... %; with 5 or more XBPs ... It is recommended not to perform more than one or two runtime calibrations per year , as frequent battery calibrations can significantly decrease the life expectancy of the battery. ... It is important to note that the actual run time during a power outage is not affected by whether a run time calibration had been performed, as the actual run time is dependent on the physical power
Creating an Aggregate Device within the KVM Access Software
... Software and why it may be suggested ... ... ships with KVMXXXX Digital IP KVMs) ... wishing to consolidate nodes within their KVM ... ... as a single node , and only ... ... together, making it easier for the ... ... I have 300 node license but have ... ... purchase a 900 node license to cover ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... ... to connect to it (via browser ... 5 .) Optional ... If it has more than ... ... , Dell DRAC 5 , Dell iDRAC ... ... will bring up its management page. ... , Dell DRAC 5 , Dell iDRAC ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... Please be sure it is the same ... ... has licensing on it (beyond the base 25 device nodes and 1 surveillance node ) your will ... 5 ) During deployment of the trial VM, please be sure to add a second NIC card to accommodate the private LAN NIC from the hardware server and add a second hard drive to at least match the hard drive space of the hardware from which you are deploying. ... 7) Verify the mac address of the new VM and register it at https://dcimassets.schneider-electric.com.
What is the expected life of my APC UPS battery?
... is 20- 25 ° ... last for 4 years at 25 ° ... good for 2 years if operated at ... ... two times a year , if necessary ... It is also important ... ... be used or it will lose a great deal of its charge . It is not advisable ... If the ambient temperature during storage is - 15°C to + 30°C (+ 5 °F to + 86°F), perform a full recharge cycle at least every six months. ... It is not recommended that the load exceed 80 percent of the UPS unit’s rated capacity.


Résultats 1 - 10 de 70

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.