Consulter la FAQ



Data Center Expert | How do hardware and software support contracts work?
... work for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... StruxureWare Data Center Expert appliances come with ... The Data Center Expert appliance and any ... ... a default 25 nodes (covered under ... as each additional node license . Modbus license keys and surveillance keys do not ... StruxureWare Data Center Expert Appliances can have ... a total of 5 years, which ... Year 5 ... your server and license keys back under ... ... amount of Device Nodes Installed ... number of install licenses .
Data Center Expert | What virtualization environments are supported?
... supported for the Data Center Expert virtual appliance? StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all verisons ... ... The most recent information on supported virtualization ... EcoStruxure IT Help Center at: ... /360039289653- Data - Center - Expert -Virtual- ... The Data Center Expert v7. ... ... monitors up to five device nodes and one surveillance node . ... can purchase a license key to upgrade ... monitor additional device nodes and activate supported ... ... development of the Data Center Expert 7.2 ... The Data Center Expert virtual appliance is delivered as an OVA ( ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... As the data center is moving away ... ... server already has licensing on it ( ... base 25 device nodes and 1 surveillance node ) your will ... License keys are tied ... ... contracts for the license keys and the ... can reset the license key passcodes so ... used again to license the virtual server ... ... new servers/ licenses . 5 ) During deployment ... Register the passcodes obtained from tech support for the license keys against this mac address. ... 9) Import the license keys (starting with the VM activation key) created from the previous registration step.
Data Center Expert | Getting Started
... started with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... Deploying the Physical Data Center Expert Appliance ... Deploying the Virtual Data Center Expert Appliance ... is restricted to 5 nodes . ... you have purchased licensing , continue to ... the passcodes for licenses . ... deploy the StruxureWare Data Center Expert Virtual Appliance? ... of storage that Data Center Expert has within VMWare ... Getting Data Center Expert on the Network ... ensuring that your Data Center Expert (DCE) ... ... Settings for StruxureWare Data Center Expert
Data Center Expert | Trial version VM appears to have 25 nodes available.
... Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to ...
Video: How do I retrieve surveillance clips in StruxureWare Data Center Expert
Retrieving surveillance clips in StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (DCE) NetBotz discovered by DCE and licensed for surveillance ... 1) Open the DCE Client and go to the Surveillance perspective. ... If a thumbnail shows a red circle with a cross-line through it, the camera has not been licensed for surveillance . ... 5 ) Within the Choose Date section, select either Relative or Date Range.
Unlicensing a Camera from NetBotz Central Results in Deletion of Associated Surveillance Pictures
... Deletion of Associated Surveillance Picture. StruxureWare Data Center Expert ... Central/ StruxureWare Data Center Expert Surveillance , any existing Surveillance pictures associated with ... To retain the historical Surveillance pictures for a camera without having it posted future Surveillance pictures to the server, set "Post Mode" to 'Disabled' in Modify Camera Surveillance Settings. This way, no more new Surveillance pictures are generated from the camera, and users can still review past Surveillance pictures associated with this camera. Note that only unlicensing cameras can free up Surveillance license nodes .
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions ... SturuxureWare Data Center Expert requires a 64 character license key that is ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... to gather specific information about the alert ... ... when purchasing a license key is not the actual license . ... passcode to a license key. 5 . To add ... ... AP9465 = StruxureWare Data Center Expert Basic ... ap9470 = StruxureWare Data Center Expert Standard ... AP9475 = StruxureWare Data Center Expert Enterprise
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
Each NetBotz camera requires one Surveillance license .
Data Center Expert | Surveillance frame rate when NetBotz communication is SSL
... set within the Data Center Expert surveillance settings, the maximum frame rate Data Center Expert will receive from ... NetBotz appliance is 5 frames per second ...


Résultats 1 - 10 de 56

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.