FAQs Techniques

Poser une question

Filtre de Résultat

    Video: Data Center Expert | How do I delete old data?
    ... from StruxureWare Data Center Expert StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Resolution : Accessing Purge Settings Accessing Data Center Expert Purge Settings ... > Server Administration Settings > Storage Settings > Purge Settings Automatic Purge Settings Data Center Expert is set by default to ... ... that can be set for purging data ... ... percentage of total capacity that will initiate ... ... percentage of total capacity that will cause ... ... percentage of total capacity that will result ... ... the StruxureWare Data Center Expert Administrators that ... Apply Purge Settings Click to save changes to the settings . Data Center Expert storage repositories ...
    Netbotz / InfraStruXure Central supplemental OID configuration
    Netbotz / InfraStruXure Central supplemental OID configuration ... StruxureWare Data Center Expert ... InfraStruxure Central/Data Center Expert, any version ... When configuring Netbotz products to monitor SNMP devices through device scanners or device crawlers, there is an option for "Supplemental OIDs". ... Resolution : ... The OID below is a sample that would return the Battery Capacity of an APC UPS:
    How to install and setup the StruxureOn Gateway
    How to install and setup the StruxureOn Gateway Resolution 1. Downloading and installing the Gateway Download and install the Gateway from ... 2. Setting up a proxy server ... , specify the settings . Click Proxy Settings ... automatically detect proxy settings or configure the settings manually. ... server using these settings . After you install StruxureOn Gateway, ... 3. Discovering devices ... After you have installed the StruxureOn Gateway ... you need to set up which devices you ... 5. Inviting users ... of the initial setup process or any ... ... and perform additional configuration , such as configuring alarm thresholds, configuring device polling interval ... 6. Setting up call priority ... for your data center , to get ... ... drop users to set up or edit the ...
    Before importing a backup from a StruxureWare Data Center Expert server to the Virtual Appliance version, configure the public and private network settings first in VMWare.
    Issue: Before importing a backup from a StruxureWare DCE server to the Virtual Appliance version, configure the public and private network settings first in VMWare
    How do I mass configure APC user settings using Data Center Expert?
    Mass Configure User Settings on 3.X-5.X NMCs
    Video: Data Center Expert | How do I configure the network settings?
    Upon initial setup , DCE requires that the network settings (IP Address, Subnet mask, Gateway, DNS Servers, and Hostname) ...
    Data Center Expert | Using APC SNMP Device Configuration to change SNMP settings may disassociate the current notification policy for that device.
    After using APC SNMP Device Configuration , for an SNMP settings change or a migration from snmpv1 to snmpv3, check the notification policies and ...
    StruxureWare Data Center Expert message stuck retrieving configuration
    ... pushing some values related to FTP through the APC SNMP device configuration that DCE does not update it's service configuration settings .
    Video: Data Center Expert | How do I mass configure APC devices?
    FA317377 If you wish to mass configure user settings (username & password), see knowledge base .
    Setting Up IPMI on StruxureWare Data Center Expert Enterprise
    The following settings should be configured :
    Résultats 1 - 10 de 75